SC16IS741A wont sleep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS741A wont sleep

638 Views
willdamerell
Contributor I

Hi ,

      For our application we are sending very small packets of data (50 Bytes) very infrequently hence the

SC16IS741A should be asleep for 99.9% of the time.

Our problem is we cant get it to sleep.

Please can you confirm the registers that we should be setting over SPI to put it to sleep.

Attached is a Jpeg showing the settings that we are applying.

Best regards

Will

0 Kudos
1 Reply

567 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Will,

First two transactions are correct, but the IER register is accessible only when LCR[7] = 0. So you need to clear this bit first and then send 0x0810 to set the IER[4] bit.

Hope it helps.

Best regards,

Tomas

0 Kudos