Regarding to DisplayPort to VGA adapter, is the PTN3392 suitable for motherboard
applications?
I mean to convert a DisplayPort signal directly from CPU(not from the Displayport conenector!)
to an analog video signal that connects to the VGA connector?
The CPU i am using is Skylake E3-1268L v5 which has the Dual mode DP++ ports...
By the way, PTN3355 is more suitable for the above appilcation?