I have some problem about MMA8652's low power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have some problem about MMA8652's low power

545 Views
ipx002
Contributor I

Hi

    I have some problem about MMA8652 . I set the ODR=1.56(CTRL_REG1=0x38) , and work in low power mode(CTRL_REG2=0x1b) . It's current should be 6.5 uA.

    pastedImage_3.png

   But I read the current is 170 uA with digital ammeter . Why?

pastedImage_4.png

And my Schematic like that

pastedImage_5.png

my code is

IIC_write(CTRL_REG1,0x38);              //ODR = 1.56Hz, standby

IIC_write(XYZ_DATA_CFG_REG,0x02);       //+/-8g

IIC_write(CTRL_REG2,0x1b);              //Low Power

  IIC_write(PULSE_CFG_REG, 0x15);         //Enable X, Y and Z Single Pulse

  IIC_write(PULSE_THSX_REG, 0x78);        //Set X Threshold to 7.56g

  IIC_write(PULSE_THSY_REG, 0x78);        //Set Y Threshold to 7.56g

  IIC_write(PULSE_THSZ_REG, 0x78);        //Set Z Threshold to 7.56g

 

  IIC_write(PULSE_TMLT_REG, 0x28);        //Set Time Limit for Tap Detection to 25 ms

  IIC_write(PULSE_LTCY_REG, 0x28);        //Set Latency Time to 50 ms

  IIC_write(CTRL_REG4, 0x08);             //Pulse detection interrupt enabled

  IIC_write(CTRL_REG5, 0x08);             //Route INT1 to system interrupt

  data = IIC_read(CTRL_REG1);   //Active Mode

  data |= 0x01;

  IIC_write(CTRL_REG1, data);

Thank you ! every body!

0 Kudos
2 Replies

368 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jun,

How are you measuring this current consumption? Are not there other devices drawing current as well?

Also be aware that the current consumption stated in the datasheet applies for VDD=2.5V and has been measured with an amperemeter between 2.5V voltage rail and VDD input only.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos

368 Views
ipx002
Contributor I

Hi Tomas

    Thank you for you reply !

     I already know the reason . Because the  MCU's IIC isn't working , so the sensor's register use default value .

     This is my fault !

     Thanks again !

     (PS: I am chineses. My family name is "Wu" , not "Jun"..haha...)

0 Kudos