Hi, all.
I wonder a part of below circuits.
(That is 4 page SABRE BD circuits of CPU Bd about i.MX6 Dual lite.)
'C2' is '220uF/25V Electoltytic-capacitor'.
I think '220uF' is too many value.
Is it special reason to use '220uF Elec-Cap' for 'C2'?
And, Is it possible '100uF' of '47uF' for 'C2'?
Please, Infome me that reason.
Best Regards,
Inho Jeon.
Hi Inho
seems 'C2' could be reduced if quality power supply
is used (on J8 DC_JACK, sch-27767), this can be evaluated with
oscilloscope measuring ripples, <5% would be sufficient.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------