Can all the L2 Eth interfaces in the T1040 be used as 10/100 Mbit or just GigE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can all the L2 Eth interfaces in the T1040 be used as 10/100 Mbit or just GigE?

396 Views
luisroa
Contributor I

Can all the L2 Eth interfaces in the T1040 be used as 10/100 Mbit simultaneously or just GigE?

0 Kudos
1 Reply

363 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

What do you mean as “all the L2 Eth interfaces in the T1040”? Do you mean the T1040 internal Ethernet switch?

This switch has 8 Ethernet ports, which are tri-speed 10/100/1000 Mbps ports. All these ports can be configured for 100 Mbps.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos