Hello,
I need to flash a 200+MB image to NAND, but the rootfs created on RAM by the MFGTOOL is only 120M, how can I increase this size?
Thanks
Solved! Go to Solution.
Thanks Igor!
Hi Valentina
mfg tool is small linux image which is located
in ..Profiles/Linux/OS Firmware/firmware.
Images which are programmed on board are located
in ..Profiles/Linux/OS Firmware/files, seems there should be
no problem with its size. These images are build independently
from mfg tool.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
my question is different, when the mfgtool image boots and creates the ram image, the space available in the rootfs is only 120MiB, 20MiBare used by the files and thus only a 100MiB image can be stored in /tmp to flash the nand. I need the rootfs in RAM to be at least 200MiB
my rootfs.ubi is around 200MiB, when my mfgtool script (ucl.xml) sends the file via USB, the file won't fit the temporary file system created by the mfgtool firmware, I need this file system to be 200MiB