Content originally posted in LPCWare by lsqspb on Wed Sep 04 01:06:18 MST 2013
Quote: capiman
Hello Zhai,
which LPCXpresso are you using?
There is usually the vector table at address 0,
so perhaps when the vector table is at address 0
and even nothing between to 0x40000, then your program starts,
i think it could be larger than 128 KBytes?
Best regards,
Martin
HI Martin:
At address 0 has boot loader program, it will make the program run correctly, But I can't debug, The LPCXpresso says that "Could not start execution from stop: Ep(-1). PC is out of allowed range ". The LPCXpresso version is LPCXpresso v5.2.4_2122.