Content originally posted in LPCWare by zepedrowdp on Tue May 06 07:30:29 MST 2014 Hello,
I was able to modify the MCB1700 emWin BSP and compile it in order for it to work on my custom board (using LPC1754 and a 2.4'' TFT with ILI9341).
I got one warning "Invalid project path: Missing profject folder or file [name of the project]\Setup for Source path", that I have no idea where it's comming from. (I already tried to rename the .sc file on metadata folder with no success).
When I try to debug, the program always stops on GUI_Init() (called by the MainTask() ) and I guet a message saying "No source available for "GUI_Init() at 0xa3de" " as well as on GUI_Config() (No source available for "GUI_Init() at 0xa3de" ).
It appears to be something related with the functions: