linker script and startup code - GCC ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linker script and startup code - GCC ARM

14,031 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregUR on Wed Oct 10 01:38:21 MST 2012
Hi
I can build a simple code by GCC for ARM, and I am trying to run it on MCB4300 with gdbserver and arm-none-eabi.gdb. The linker script and startup code are taken from CMSIS v3 (Device/ARM/ARMCM4/Source/GCC/startup_ARMCM4.S and Device/ARM/ARMCM4/Source/GCC/gcc_arm.ld) without modifications, but I also tried to modify flash and RAM addresses in .ld file.

It builds without problems with this command:

./arm-none-eabi-gcc -g -mthumb -mcpu=cortex-m4 -march=armv7e-m -T Device/ARM/ARMCM4/Source/GCC/gcc_arm.ld Device/ARM/ARMCM4/Source/GCC/startup_ARMCM4.S main.c -o out.elf

I have to ctrl+c because it never gets to the breakpoint. Instead, it goes to 0x1c000206, but breakpoint is at 0x200. What are memory addresses that should be put into linker script ? Should anything else be changed in CMSIS's .ld and .s files ?

Output of arm-none-eabi-gbd:

(gdb) target remote :2331
Remote debugging using :2331
0x00000000 in __isr_vector ()
(gdb) load
Loading section .text, size 0x50c lma 0x0
Loading section .ARM.exidx, size 0x8 lma 0x50c
Loading section .data, size 0x440 lma 0x514
Loading section .jcr, size 0x4 lma 0x954
Start address 0x17d, load size 2392
Transfer rate: 395 bytes/sec, 598 bytes/write.
(gdb) break main
Breakpoint 1 at 0x200: file main.c, line 37.
(gdb) c
Continuing.
^C
Program received signal SIGTRAP, Trace/breakpoint trap.
0x1c000206 in ?? ()
(gdb)


and from gdbserver:

SEGGER J-Link GDB Server V4.50i

JLinkARM.dll V4.50i (DLL compiled Jun 22 2012 19:00:36)

The server has been started with the following settings:
---Server related settings---
GDBInit file:              none
Listening port:            2331
SWO thread listening port: 2332
Accept remote connection:  yes
Logfile:                   off
Verify download:           off
Init regs on start:        on
Silent mode:               off
Single run mode:           off
---J-Link related settings---
J-Link script:             none
Target interface:          JTAG
Host interface:            USB
Target endian:             little
Target interface speed:    5kHz

Waiting for J-Link connection...
J-Link is connected.
Firmware: J-Link ARM V8 compiled Aug  1 2012 13:40:47
Hardware: V8.00
S/N: 158007019
OEM: IAR
Checking target voltage...
Listening on TCP/IP port 2331
Connecting to target...
J-Link found 2 JTAG devices, Total IRLen = 8
JTAG ID: 0x4BA00477 (Cortex-M4)
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x00000000 (Data = 0x1000BEC8)
Downloading 1292 bytes @ address 0x00000000
Downloading 8 bytes @ address 0x0000050C
Downloading 1088 bytes @ address 0x00000514
Downloading 4 bytes @ address 0x00000954
Writing register (PC = 0x0000017d)
Read 4 bytes @ address 0x0000017C (Data = 0x4B01F810)
Read 2 bytes @ address 0x00000200 (Data = 0x4809)
Read 2 bytes @ address 0x00000200 (Data = 0x4809)
Read 2 bytes @ address 0x00000200 (Data = 0x4809)
Setting breakpoint @ address 0x00000200, Size = 2, BPHandle = 0x0001
Starting target CPU...
Debugger requested to halt target...
...Target halted (PC = 0x1C000206)
Reading all registers
Removing breakpoint @ address 0x00000200, Size = 2
Read 4 bytes @ address 0x1C000206 (Data = 0xE7FEE7FE)

main.c:

int globalVar = 0;

void SystemInit (void) {

#if 0
uint32_t    SystemCoreClock = __IRC;
#ifdef __CODE_RED
    // CodeRed startup code will modify VTOR register to match
    // when code has been linked to run from.

    // Check whether we are running from external flash
    if (SCB->VTOR == 0x1C000000)
        /*Enable Buffer for External Flash*/
        LPC_EMC->STATICCONFIG0 |= 1<<19;

    // Call clock initialisation code
    CGU_Init();

#else

#if defined(CORE_M4) || defined(CORE_M3)
        // Enable VTOR register to point to vector table
        SCB->VTOR = getPC() & 0xFFF00000;
#endif

    /*Enable Buffer for External Flash*/
    LPC_EMC->STATICCONFIG0 |= 1<<19;
#endif
#endif
}

int main(void)
{
  int i;
  while(1)
    globalVar++;
  return 0;
}

startup_ARMCM4.S:

/* File: startup_ARMCM4.S
* Purpose: startup file for Cortex-M4 devices. Should use with
*   GCC for ARM Embedded Processors
* Version: V1.3
* Date: 08 Feb 2012
*
* Copyright (c) 2012, ARM Limited
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions are met:
    * Redistributions of source code must retain the above copyright
      notice, this list of conditions and the following disclaimer.
    * Redistributions in binary form must reproduce the above copyright
      notice, this list of conditions and the following disclaimer in the
      documentation and/or other materials provided with the distribution.
    * Neither the name of the ARM Limited nor the
      names of its contributors may be used to endorse or promote products
      derived from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND
* ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
* WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
* DISCLAIMED. IN NO EVENT SHALL ARM LIMITED BE LIABLE FOR ANY
* DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
* LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND
* ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
* SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
    .syntax unified
    .arch armv7-m

    .section .stack
    .align 3
#ifdef __STACK_SIZE
    .equ    Stack_Size, __STACK_SIZE
#else
    .equ    Stack_Size, 0x400
#endif
    .globl    __StackTop
    .globl    __StackLimit
__StackLimit:
    .space    Stack_Size
    .size __StackLimit, . - __StackLimit
__StackTop:
    .size __StackTop, . - __StackTop

    .section .heap
    .align 3
#ifdef __HEAP_SIZE
    .equ    Heap_Size, __HEAP_SIZE
#else
    .equ    Heap_Size, 0xC00
#endif
    .globl    __HeapBase
    .globl    __HeapLimit
__HeapBase:
    .if    Heap_Size
    .space    Heap_Size
    .endif
    .size __HeapBase, . - __HeapBase
__HeapLimit:
    .size __HeapLimit, . - __HeapLimit

    .section .isr_vector
    .align 2
    .globl __isr_vector
__isr_vector:
    .long    __StackTop            /* Top of Stack */
    .long    Reset_Handler         /* Reset Handler */
    .long    NMI_Handler           /* NMI Handler */
    .long    HardFault_Handler     /* Hard Fault Handler */
    .long    MemManage_Handler     /* MPU Fault Handler */
    .long    BusFault_Handler      /* Bus Fault Handler */
    .long    UsageFault_Handler    /* Usage Fault Handler */
    .long    0                     /* Reserved */
    .long    0                     /* Reserved */
    .long    0                     /* Reserved */
    .long    0                     /* Reserved */
    .long    SVC_Handler           /* SVCall Handler */
    .long    DebugMon_Handler      /* Debug Monitor Handler */
    .long    0                     /* Reserved */
    .long    PendSV_Handler        /* PendSV Handler */
    .long    SysTick_Handler       /* SysTick Handler */

    /* External interrupts */
    .long    WDT_IRQHandler        /*  0:  Watchdog Timer            */
    .long    RTC_IRQHandler        /*  1:  Real Time Clock           */
    .long    TIM0_IRQHandler       /*  2:  Timer0 / Timer1           */
    .long    TIM2_IRQHandler       /*  3:  Timer2 / Timer3           */
    .long    MCIA_IRQHandler       /*  4:  MCIa                      */
    .long    MCIB_IRQHandler       /*  5:  MCIb                      */
    .long    UART0_IRQHandler      /*  6:  UART0 - DUT FPGA          */
    .long    UART1_IRQHandler      /*  7:  UART1 - DUT FPGA          */
    .long    UART2_IRQHandler      /*  8:  UART2 - DUT FPGA          */
    .long    UART4_IRQHandler      /*  9:  UART4 - not connected     */
    .long    AACI_IRQHandler       /* 10: AACI / AC97                */
    .long    CLCD_IRQHandler       /* 11: CLCD Combined Interrupt    */
    .long    ENET_IRQHandler       /* 12: Ethernet                   */
    .long    USBDC_IRQHandler      /* 13: USB Device                 */
    .long    USBHC_IRQHandler      /* 14: USB Host Controller        */
    .long    CHLCD_IRQHandler      /* 15: Character LCD              */
    .long    FLEXRAY_IRQHandler    /* 16: Flexray                    */
    .long    CAN_IRQHandler        /* 17: CAN                        */
    .long    LIN_IRQHandler        /* 18: LIN                        */
    .long    I2C_IRQHandler        /* 19: I2C ADC/DAC                */
    .long    0                     /* 20: Reserved                   */
    .long    0                     /* 21: Reserved                   */
    .long    0                     /* 22: Reserved                   */
    .long    0                     /* 23: Reserved                   */
    .long    0                     /* 24: Reserved                   */
    .long    0                     /* 25: Reserved                   */
    .long    0                     /* 26: Reserved                   */
    .long    0                     /* 27: Reserved                   */
    .long    CPU_CLCD_IRQHandler   /* 28: Reserved - CPU FPGA CLCD   */
    .long    0                     /* 29: Reserved - CPU FPGA        */
    .long    UART3_IRQHandler      /* 30: UART3    - CPU FPGA        */
    .long    SPI_IRQHandler        /* 31: SPI Touchscreen - CPU FPGA */

    .size    __isr_vector, . - __isr_vector

    .text
    .thumb
    .thumb_func
    .align 2
    .globl    Reset_Handler
    .type    Reset_Handler, %function
Reset_Handler:
/*     Loop to copy data from read only memory to RAM. The ranges
*      of copy from/to are specified by following symbols evaluated in
*      linker script.
*      __etext: End of code section, i.e., begin of data sections to copy from.
*      __data_start__/__data_end__: RAM address range that data should be
*      copied to. Both must be aligned to 4 bytes boundary.  */

    ldr    r1, =__etext
    ldr    r2, =__data_start__
    ldr    r3, =__data_end__

#if 1
/* Here are two copies of loop implemenations. First one favors code size
* and the second one favors performance. Default uses the first one.
* Change to "#if 0" to use the second one */
.flash_to_ram_loop:
    cmp     r2, r3
    ittt    lt
    ldrlt   r0, [r1], #4
    strlt   r0, [r2], #4
    blt    .flash_to_ram_loop
#else
    subs    r3, r2
    ble    .flash_to_ram_loop_end
.flash_to_ram_loop:
    subs    r3, #4
    ldr    r0, [r1, r3]
    str    r0, [r2, r3]
    bgt    .flash_to_ram_loop
.flash_to_ram_loop_end:
#endif

#ifndef __NO_SYSTEM_INIT
    ldr    r0, =SystemInit
    blx    r0
#endif

    ldr    r0, =_start
    bx    r0
    .pool
    .size Reset_Handler, . - Reset_Handler

/*    Macro to define default handlers. Default handler
*    will be weak symbol and just dead loops. They can be
*    overwritten by other handlers */
    .macro    def_irq_handler    handler_name
    .align 1
    .thumb_func
    .weak    \handler_name
    .type    \handler_name, %function
\handler_name :
    b    .
    .size    \handler_name, . - \handler_name
    .endm

    def_irq_handler    NMI_Handler
    def_irq_handler    HardFault_Handler
    def_irq_handler    MemManage_Handler
    def_irq_handler    BusFault_Handler
    def_irq_handler    UsageFault_Handler
    def_irq_handler    SVC_Handler
    def_irq_handler    DebugMon_Handler
    def_irq_handler    PendSV_Handler
    def_irq_handler    SysTick_Handler
    def_irq_handler    Default_Handler

    def_irq_handler    WDT_IRQHandler
    def_irq_handler    RTC_IRQHandler
    def_irq_handler    TIM0_IRQHandler
    def_irq_handler    TIM2_IRQHandler
    def_irq_handler    MCIA_IRQHandler
    def_irq_handler    MCIB_IRQHandler
    def_irq_handler    UART0_IRQHandler
    def_irq_handler    UART1_IRQHandler
    def_irq_handler    UART2_IRQHandler
    def_irq_handler    UART3_IRQHandler
    def_irq_handler    UART4_IRQHandler
    def_irq_handler    AACI_IRQHandler
    def_irq_handler    CLCD_IRQHandler
    def_irq_handler    ENET_IRQHandler
    def_irq_handler    USBDC_IRQHandler
    def_irq_handler    USBHC_IRQHandler
    def_irq_handler    CHLCD_IRQHandler
    def_irq_handler    FLEXRAY_IRQHandler
    def_irq_handler    CAN_IRQHandler
    def_irq_handler    LIN_IRQHandler
    def_irq_handler    I2C_IRQHandler
    def_irq_handler    CPU_CLCD_IRQHandler
    def_irq_handler    SPI_IRQHandler

    .end


gcc_arm.ld:

/* Linker script to configure memory regions. */
MEMORY
{
  FLASH (rx) : ORIGIN = 0x00000000, LENGTH = 0x40000   /* 256k */
  RAM (rwx)  : ORIGIN = 0x20000000, LENGTH = 0x08000   /*  32k */
}

/* Library configurations */
GROUP(libgcc.a libc.a libm.a libnosys.a)

/* Linker script to place sections and symbol values. Should be used together
* with other linker script that defines memory regions FLASH and RAM.
* It references following symbols, which must be defined in code:
*   Reset_Handler : Entry of reset handler
*
* It defines following symbols, which code can use without definition:
*   __exidx_start
*   __exidx_end
*   __etext
*   __data_start__
*   __preinit_array_start
*   __preinit_array_end
*   __init_array_start
*   __init_array_end
*   __fini_array_start
*   __fini_array_end
*   __data_end__
*   __bss_start__
*   __bss_end__
*   __end__
*   end
*   __HeapLimit
*   __StackLimit
*   __StackTop
*   __stack
*/
ENTRY(Reset_Handler)

SECTIONS
{
.text :
{
KEEP(*(.isr_vector))
*(.text*)

KEEP(*(.init))
KEEP(*(.fini))

/* .ctors */
*crtbegin.o(.ctors)
*crtbegin?.o(.ctors)
*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)
*(SORT(.ctors.*))
*(.ctors)

/* .dtors */
*crtbegin.o(.dtors)
*crtbegin?.o(.dtors)
*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)
*(SORT(.dtors.*))
*(.dtors)

*(.rodata*)

KEEP(*(.eh_frame*))
} > FLASH

.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > FLASH

__exidx_start = .;
.ARM.exidx :
{
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
} > FLASH
__exidx_end = .;

__etext = .;

.data : AT (__etext)
{
__data_start__ = .;
*(vtable)
*(.data*)

. = ALIGN(4);
/* preinit data */
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP(*(.preinit_array))
PROVIDE_HIDDEN (__preinit_array_end = .);

. = ALIGN(4);
/* init data */
PROVIDE_HIDDEN (__init_array_start = .);
KEEP(*(SORT(.init_array.*)))
KEEP(*(.init_array))
PROVIDE_HIDDEN (__init_array_end = .);


. = ALIGN(4);
/* finit data */
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP(*(SORT(.fini_array.*)))
KEEP(*(.fini_array))
PROVIDE_HIDDEN (__fini_array_end = .);

. = ALIGN(4);
/* All data end */
__data_end__ = .;

} > RAM

.bss :
{
__bss_start__ = .;
*(.bss*)
*(COMMON)
__bss_end__ = .;
} > RAM

.heap :
{
__end__ = .;
end = __end__;
*(.heap*)
__HeapLimit = .;
} > RAM

/* .stack_dummy section doesn't contains any symbols. It is only
* used for linker to calculate size of stack sections, and assign
* values to stack symbols later */
.stack_dummy :
{
*(.stack)
} > RAM

/* Set stack top to end of RAM, and stack limit move down by
* size of stack_dummy section */
__StackTop = ORIGIN(RAM) + LENGTH(RAM);
__StackLimit = __StackTop - SIZEOF(.stack_dummy);
PROVIDE(__stack = __StackTop);

/* Check if data + heap + stack exceeds RAM limit */
ASSERT(__StackLimit >= __HeapLimit, "region RAM overflowed with stack")
}
Labels (1)
0 Kudos
Reply
1 Reply

5,432 Views
Ukhan
Contributor I

Hi @lpcware ,

Had you managed to resolve the issue? I've been encountering a similar situation for about a week now, and I'm unsure of what might be causing it.

Regards,

0 Kudos
Reply