Content originally posted in LPCWare by FrankAndersen on Mon Feb 15 07:42:07 MST 2016
Hi,
I have a program, that uses IAP for updating itself, I know it is with the risk of making it to a brick.
But untill now it has been working fine, but I now need to run the core at 96 MHz instead of 48 MHz.
I did change Param2 to 96000.
Sometimes it does not erase other times it does erase but does not write everything to the internal flash.
It looks like it makes a reset, in the middle of it all.
Any suggestions?
Best regards,