I am connecting ublox m8 device to LS1021a-iot board which will send gps data in NMEA format to LS1021aiot board.
I want to know is their any way through which I can read gps data which is in NMEA data from ublox m8 device?
NMEA is frame format only, it does not define hardware (signaling) protocol.
According to the information I was able to find in Internet for "u-blox M8" keyword, this device supports several type of serial communication ports - DDC (I2C-like), UART, USB and SPI. Our LS1021A processor support any of these protocols.
Please refer to Chapter 10 "Serial Communication Ports Description" of the below document for more information:
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------