Hello,
do You mean OCRAM ?
Regards,
Yuri.
Hi Yuri,
Let me explain a bit more. We have an imx6 design which can boot from either eMMC or from a microSD card (there is a switch to choose which to boot from). I would like to add another bootloader which runs first - this one will be in the imx6 on board flash. This pre-bootloader will look at the image on the eMMC and the image on the microSD and decide which one to boot from. Currently my u-boot image is about 320kb so I am not sure if I can strip it down to less than 96k to fit into the imx flash.
On the old LTIB system there was a smaller bootloader called Redboot for this purpose, but I don't think it's there in the Yocto system.
Any advice appreciated!
Cheers,
Neil.
Hello,
i.MX6 boot ROM is mask programmed - it cannot be changed by customers.
Regards,
Yuri.
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
------------------------------------------------------------------------------