SGTL5000 and Reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 and Reset

693 Views
pinkesh
Contributor I

Hello  Everyone,We have configured SGTL as below .

Provided SYS_MCLK = 12 MHz from custom board which runs without any OS and SGTL as I2S master with sample frequency equal to 8 KHz .

In our scenario , If reset event occurred due to Watchdog timer, We are not able to configure SGTL again .

Is there any work-around so that we can reset/reconfigure SGTL after controller reset event  ?

- Pinkesh

Tags (1)
0 Kudos
1 Reply

506 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pinkesh

please try patch below

ASoC: sgtl5000: Fix driver probe after reset · wandboard-org/linux@a648586 · GitHub

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos