Hi,
I would like to access to the NOR flash in the t2080rdb from Linux.
Is it that possible?
Can I format those flashs in any format? for example fat or ext2 or ext4? I don´t care if it is not advisable. I just want to know if it is possible and how to access to the information form Linux.
BR
Solved! Go to Solution.
Hello manolo ruiz,
First please make sure that IFC NOR driver has been configured in Kernel, in T2080RDB default dts file no partitions defined for NOR Flash, you could add partition definition in the node "nor@0,0" in the file t208xrdb.dtsi similar as the following, and rebuild the dts file.
nor@0,0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "cfi-flash";
reg = <0x0 0x0 0x8000000>;
bank-width = <2>;
device-width = <1>;
partition@800000 {
/* 1Mor DTB Image */
reg = <0x08000000 0x00100000>;
label = "NOR DTB Image";
};
partition@20000 {
/* 7 MB for Linux Kernel Image */
reg = <0x00020000 0x00700000>;
label = "NOR Linux Kernel Image";
};
partition@1300000 {
/* 20MB for JFFS2 based Root file System */
reg = <0x01300000 0x01400000>;
label = "NOR JFFS2 Root File System";
};
... ...
}
To verify NOR flash device as the following after the system boot up.
[root@ root]# cat /proc/mtd
dev: size erasesize name
mtd0: 00800000 000100000 "NOR DTB Image"
mtd1: 00020000 00700000 "NOR Linux Kernel Image"
mtd3: 01300000 01400000 "NOR JFFS2 Root File System"
[root@ root]# flash_eraseall -j /dev/mtd2
Erasing 128 Kibyte @ 1400000 -- 100% complete. Cleanmarker written at 13e0000.
[root@P1010RDB root]# mount -t jffs2 /dev/mtdblock2 /mnt
JFFS2 notice: (1202) jffs2_build_xattr_subsystem: complete building xattr subsystem, 0 of
xdatum (0 unchecked, 0 orphan) and 0 of xref (0 dead, 0 orphan) found.
[root@ root]# cd /mnt/
[root@ mnt]# ls -l
[root@ mnt]# touch flash_file
[root@ root]# umount mnt
Or use the following commands
# mtd_debug erase /dev/mtd2 0 <mtdblack_size>
# mkfs.ext2 /dev/mtdblock2
# mount -t ext2 /dev/mtd2 /mnt
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello manolo ruiz,
First please make sure that IFC NOR driver has been configured in Kernel, in T2080RDB default dts file no partitions defined for NOR Flash, you could add partition definition in the node "nor@0,0" in the file t208xrdb.dtsi similar as the following, and rebuild the dts file.
nor@0,0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "cfi-flash";
reg = <0x0 0x0 0x8000000>;
bank-width = <2>;
device-width = <1>;
partition@800000 {
/* 1Mor DTB Image */
reg = <0x08000000 0x00100000>;
label = "NOR DTB Image";
};
partition@20000 {
/* 7 MB for Linux Kernel Image */
reg = <0x00020000 0x00700000>;
label = "NOR Linux Kernel Image";
};
partition@1300000 {
/* 20MB for JFFS2 based Root file System */
reg = <0x01300000 0x01400000>;
label = "NOR JFFS2 Root File System";
};
... ...
}
To verify NOR flash device as the following after the system boot up.
[root@ root]# cat /proc/mtd
dev: size erasesize name
mtd0: 00800000 000100000 "NOR DTB Image"
mtd1: 00020000 00700000 "NOR Linux Kernel Image"
mtd3: 01300000 01400000 "NOR JFFS2 Root File System"
[root@ root]# flash_eraseall -j /dev/mtd2
Erasing 128 Kibyte @ 1400000 -- 100% complete. Cleanmarker written at 13e0000.
[root@P1010RDB root]# mount -t jffs2 /dev/mtdblock2 /mnt
JFFS2 notice: (1202) jffs2_build_xattr_subsystem: complete building xattr subsystem, 0 of
xdatum (0 unchecked, 0 orphan) and 0 of xref (0 dead, 0 orphan) found.
[root@ root]# cd /mnt/
[root@ mnt]# ls -l
[root@ mnt]# touch flash_file
[root@ root]# umount mnt
Or use the following commands
# mtd_debug erase /dev/mtd2 0 <mtdblack_size>
# mkfs.ext2 /dev/mtdblock2
# mount -t ext2 /dev/mtd2 /mnt
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------