Can you make a T1040 RDB boot on power-on?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you make a T1040 RDB boot on power-on?

704 Views
colindavidson
Contributor II

We have a T1040 RDB that we want to be able to restart remotely by cycling the power. This usually works, but if the power has been off for a while, the system won't boot until you hold the power switch in for a while.  This may be the result of an excessive power draw on startup, but in case it isn't, are there any settings (switch or NVRAM) which could affect this?

Thanks,

Colin

2 Replies

450 Views
colindavidson
Contributor II

Further information. The board occasionally hangs and won't reboot with a power cycle. The only way to start the system at this point is to hold the "power" button on the T1040 in until it is started. Don't have a real idea of how long this is.

If the system is powered off for a minute, we get into this situation.

Don't know the revision of the board as it is in a remote office and there is currently nobody there who can check it. Can this be determined via u-boot?

At the moment we are thinking excess startup power draw on the PCIe bus... I will post more as more information is obtained. It may be a few days.

0 Kudos

450 Views
ufedor
NXP Employee
NXP Employee

Which board revision is in question?

What exactly means "for a while" which corresponds to the problem case?

0 Kudos