Hi,
I am using kernel 3.10.53 on a sabresd board the interrupt of the pci express port was claimed by pcie pme driver but as you can see inthe output of lspci it should be handled by driver "Sigamtek PCIe"
It looks like it is a kernel option I have to set to fix this issue, because when I use an image build in november the irq 155 wasn't claimed by pcie pme.
The thing is I didn't have the configuration for this binary.
Does anyone of you have an idea what option I have to activate to get this fixed ?
cat /proc/interrupts
CPU0 CPU1 CPU2 CPU3
29: 444116 810725 3230723 2507477 GIC twd
34: 1 0 0 0 GIC sdma
35: 0 0 0 0 GIC VPU_JPG_IRQ
37: 0 0 0 0 GIC 2400000.ipu
38: 0 0 0 0 GIC 2400000.ipu
39: 0 0 0 0 GIC 2800000.ipu
40: 5 0 0 0 GIC 2800000.ipu
44: 0 0 0 0 GIC VPU_CODEC_IRQ
50: 0 0 0 0 GIC vdoa
55: 4849 0 0 0 GIC mmc1
56: 0 0 0 0 GIC mmc2
57: 470 0 0 0 GIC mmc3
58: 489 0 0 0 GIC 2020000.serial
68: 22 0 0 0 GIC 21a0000.i2c
69: 220 0 0 0 GIC 21a4000.i2c
70: 0 0 0 0 GIC 21a8000.i2c
72: 0 0 0 0 GIC 2184200.usb
75: 7001 0 0 0 GIC 2184000.usb
79: 0 0 0 0 GIC ssi@0202c000
87: 10 0 0 0 GIC i.MX Timer Tick
113: 0 0 0 0 GIC 20c0000.wdog
139: 0 0 0 0 GIC mmdc_1
144: 0 0 0 0 GIC mmdc_1
145: 0 0 0 0 GIC mmdc_1
146: 0 0 0 0 GIC mmdc_1
147: 0 0 0 0 GIC 20e0000.hdmi_video
150: 39833 0 0 0 GIC 2188000.ethernet
151: 0 0 0 0 GIC 2188000.ethernet
155: 0 0 0 0 GIC PCIe PME
169: 0 0 0 0 gpio-mxc microphone detect
192: 0 0 0 0 gpio-mxc 2198000.usdhc cd
194: 0 0 0 0 gpio-mxc 2194000.usdhc cd
360: 0 0 0 0 gpio-mxc headphone detect
IPI0: 0 0 0 0 CPU wakeup interrupts
IPI1: 0 0 0 0 Timer broadcast interrupts
IPI2: 2876 7104 4865 6529 Rescheduling interrupts
IPI3: 10 13 13 20 Function call interrupts
IPI4: 3 1 3 2 Single function call interrupts
IPI5: 0 0 0 0 CPU stop interrupts
Err: 0
root@sigmatek-arm:~# lspci -v
00:00.0 PCI bridge: Device 16c3:abcd (rev 01) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at 01000000 (32-bit, non-prefetchable) [size=1M]
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
Memory behind bridge: 01100000-012fffff
[virtual] Expansion ROM at 01300000 [disabled] [size=64K]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/1 Maskable+ 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [140] Virtual Channel
Kernel driver in use: pcieport
01:00.0 ACCESS Bus: Device 5112:0c00
Subsystem: Device 5112:0c00
Flags: bus master, fast devsel, latency 0, IRQ 155
Memory at 01100000 (32-bit, non-prefetchable) [size=1M]
Memory at 01200000 (32-bit, non-prefetchable) [size=1M]
Capabilities: [40] Power Management version 3
Capabilities: [48] MSI: Enable- Count=1/1 Maskable- 64bit+
Capabilities: [58] Express Endpoint, MSI 00
Capabilities: [100] Device Serial Number 00-00-00-01-01-00-0a-35
Kernel driver in use: Sigmatek PCIE
Kind regards
Wolfgang