MPC5746R BD Hardware Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746R BD Hardware Issue

366 Views
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

Customer use MPC5746R BD (MAPBGA-292 package), and find the code can be downloaded but the external oscillator is not work.
Compare the H/W with the EVB schematic, the different is the voltage of VDD_HV_FLA, it's 5V not 3.3V.
Any suggestion is appreciate.

 

Best regards,

Labels (1)
0 Kudos
1 Reply

270 Views
hongpingxu-b364
NXP Employee
NXP Employee

Problem solved!

Customer forget to supply VDD_HV_IO_JTAG.

0 Kudos