MCF5216CVF66  - I do not see a decoder in the datasheet telling me the difference between MCF5216CVF66 and MCF5216CVM66

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5216CVF66  - I do not see a decoder in the datasheet telling me the difference between MCF5216CVF66 and MCF5216CVM66

482 Views
davidriness
Contributor I

Customer has an existing design, and needs to know if they can swap one for the other

 

Thank you

Labels (1)
Tags (1)
0 Kudos
1 Reply

294 Views
TomE
Specialist II

It isn't in the Data Sheet.

This is a PACKAGING difference:

32-bit microcontroller with CAN|NXP

As far as I can tell from this limited information, "CVM" is Lead Free and "CVF" isn't.

So it might affect your production in that there may be soldering problems changing from one package to the other.

Tom

0 Kudos