TDM interface for 1043 series QorIQ processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TDM interface for 1043 series QorIQ processor

851 Views
ajaysood
Contributor I

TDM interface is critical to our product in mind since the chipsets that we intend to use are giving PCM output

Questions -

Will the TDM interface for 1043 series processor be able  to take in PCM input directly or it needs something in between?

There was a mention of TDM riser card in the documentation, is that an optional component?

Does the evaluation toolkit come with some tool  which can help us generate PCM data and drive the TDM interfaces of the processor for the time being ?

Thanks

Ajay

0 Kudos
2 Replies

495 Views
bpe
NXP Employee
NXP Employee

>Will the TDM interface for 1043 series processor be able  to take in PCM input directly or it needs something in between?

>

[Platon] It depends on the frame structure,  timing and signal voltage levels of your TDM peripheral. Refer to

QEIWRM  Chapter 22,  LS1043ARM  Section 14.3.11, LS1043A Datasheet Section 3.11.2.

>There was a mention of TDM riser card in the documentation, is that an optional component

>

[Platon] Yes, it is optional.

>Does the evaluation toolkit come with some tool  which can help us generate PCM data and drive the TDM interfaces

>of the processor for the time being ?

>

[Platon] There are no specific configuration or data generation tools. The SDK for LS1043ARDB includes a compact TDM driver

for minimum interface testing. Details can be found in the SDK Release Notes, Chapter 32.

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

495 Views
ajaysood
Contributor I

Thanks for the clarifications

Regards

Ajay

0 Kudos