why the ipu csi can handled up to 4 streams of data in imx6d.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why the ipu csi can handled up to 4 streams of data in imx6d.

377 Views
guanliangding
Contributor III

Hi, all:

     In imx6d, ipu csi is selected to get one of vc. This is a compatible design?

0 Kudos
1 Reply

295 Views
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

vc selection can be understood from i.MX6DQ RM  Chapter 19

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos