I am trying to run demos for SmartDSP OS on BSC9131RDB.
When I boot dsp image using command
/ipc/dsp_bt aic_loopback_9x31_rel.bin
I get following response
root@bsc913x:~# /ipc/dsp_bt /media/sda1/dsp/aic_loopback_9x31_rel.bin
===DSP boot Application===(1.1.02)==
SYSTEM MAP
DSP PrivArea: Addr=38000000 Size=8000000
Shared CtrlArea: Addr=37000000 Size=1000000
DSP Core0 M2: Addr=b0000000 Size=80000
DSP Core1 M2: Addr=0 Size=0
DSP M3: Addr=0 Size=0
PA CCSRBAR: Addr =ff700000 Size=100000
DSP CCSRBAR: Addr =ff600000 Size=100000
PA Shared Area: Addr=10000000 Size=f000000
DSP Shared Area: Addr=1f000000 Size=1000000
DSP READY SET
Copy Part b0000000 124b6
Copy Part b0014000 2f0c
Copy Part ff618108 4
DSP image copied
sleep 4 sec
DSP HW Sem1 value not correctly set, value=0
DSP Boot Failed, Please reset
The same result I get for other demos.
I will appriciate any help.
Alexander Polovnikov