Hello,
In the IMX6SXRM document (page 176) it states that there are "Four eCSPI (Enhanced CSPI), three of them can support up to 52 Mbps, one can be of low speed". But the low speed eCSPI port is not identified anywhere. Which eCSPI port is low speed on this device, and what is its actual speed?
Hi Damon
all i.MX6SX eCSPI modules are identical, so this is inaccuracy
in description.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------