Hi.. I am using linux ubuntu. I want to develop app for XBee devices by using CW. For Lunux I installed the CW from the following site. Installation was successful. But I am not able to launch CW. Following link I used to downlaod CW for Linux. http://www

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi.. I am using linux ubuntu. I want to develop app for XBee devices by using CW. For Lunux I installed the CW from the following site. Installation was successful. But I am not able to launch CW. Following link I used to downlaod CW for Linux. http://www

356 Views
sreenathr
Contributor I

Hi..

I am using linux ubuntu. I want to develop app for XBee devices by using CW. For Lunux I installed the CW from the following site. Installation was successful. But I am not able to launch CW. Following link I used to downlaod CW for Linux.

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LEGACY&fsrch=1&sr=1&pageNum=1

Could you please help?

 

Regards

Sreenath

Labels (1)
0 Kudos
1 Reply

268 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Sreenath R,

Which Ubuntu version are you using? Please notice that CodeWarrior 10.2 is only supported by Ubuntu 10.04 (32-bit and 64-bit).

Also, could you tell us which MCU are you planning to use?

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos