How to enable USB 3.0 in LS2085A QDS Board..?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable USB 3.0 in LS2085A QDS Board..?

Jump to solution
2,222 Views
anandhakumarm
Contributor III

Hi all,

I'm using LS2085A QDS Board for development, in this USB 3.0 port is there, but that is not getting detected when i insert a pendrive in that.. I checked that in u-boot as well as in kernel. I checked with all the usb commands available in u-boot and also checked the dmesg in kernel.. inserted and removed the pendrive continuously but there is no entries in dmesg.. Please help me to make it working..

Labels (1)
Tags (1)
1 Solution
1,566 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Anandha Kumar M,

USB 3.0 is supported since 20150515 release.

There are two USB ports on LS2085QDS, please use USB1 to do USB 3.0 verification.

About RCW, please refer to field RCW[USB] and RCW[USB3_CLK_FSEL], the default RCW provided in the SDK ISO is fine.

The following is USB 3.0 test log in u-boot with SanDisk USB 3.0 storage device.

U-Boot 2015.01Layerscape2-SDK+g551206e (Apr 04 2015 - 14:20:34)

SoC:  LS2085E (0x87010010)

Clock Configuration:

       CPU0(A57):1600 MHz  CPU1(A57):1600 MHz  CPU2(A57):1600 MHz 

       CPU3(A57):1600 MHz  CPU4(A57):1600 MHz  CPU5(A57):1600 MHz 

       CPU6(A57):1600 MHz  CPU7(A57):1600 MHz 

       Bus:      600  MHz  DDR:      1333.333 MHz     DP-DDR:   1333.333 MHz

Reset Configuration Word (RCW):

       00: 40282830 40400040 00000000 00000000

       10: 00000000 00200000 00200000 00000000

       20: 00c12980 00002580 00000000 00000000

       30: 00000e0b 00000000 00000000 00000000

       40: 00000000 00000000 00000000 00000000

       50: 00000000 00000000 00000000 00000000

       60: 00000000 00000000 00027000 00000000

       70: 492a0000 00000000 00000000 00000000

Board: LS2085E-QDS, Board Arch: V1, Board version: B, boot from vBank: 4

FPGA: v7 (LS2085AQDS_2015_0407_1232), build 169 on Tue Apr 07 16:32:55 2015

SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz

SERDES2 Reference : Clock1 = 100 separate SSCGMHz Clock2 = 100 separate SSCGMHz

I2C:   ready

DRAM:  Initializing DDR....using SPD

Detected UDIMM 18ASF1G72AZ-2G1A1

Detected UDIMM 18ASF1G72AZ-2G1A1

DP-DDR:  Detected UDIMM 18ASF1G72AZ-2G1A1

19.5 GiB

DDR    15.5 GiB (DDR4, 64-bit, CL=9, ECC on)

       DDR Controller Interleaving Mode: 256B

       DDR Chip-Select Interleaving Mode: CS0+CS1

DP-DDR 4 GiB (DDR4, 32-bit, CL=9, ECC on)

       DDR Chip-Select Interleaving Mode: CS0+CS1

Waking secondary cores to start from fff18000

All (8) cores are up.

Using SERDES1 Protocol: 42 (0x2a)

Using SERDES2 Protocol: 73 (0x49)

Flash: 128 MiB

NAND:  512 MiB

MMC:   FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: disabled

PCIe2: disabled

PCIe3: disabled

PCIe4: Root Complex x1 gen1, regs @ 0x3700000

     01:00.0    - 8086:107d - Network controller

PCIe4: Bus 00 - 01

In:    serial

Out:   serial

Err:   serial

Target spinup took 0 ms.

AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst

Found 1 device(s).

SCSI:  Net:   qds: WRIOP: Supported SerDes Protocol 0x2a

qds: WRIOP: Supported SerDes Protocol 0x49

mdio_register: non unique device name 'FSL_MDIO1'

Phy 28 not found

PHY reset timed out

Phy 29 not found

PHY reset timed out

Phy 30 not found

PHY reset timed out

Phy 31 not found

PHY reset timed out

crc32+

fsl-mc: Booting Management Complex ... SUCCESS

fsl-mc: Management Complex booted (version: 6.0.4, boot status: 0x1)

fsl-mc: Deploying data path layout ... SUCCESS

e1000: 00:15:17:8e:7e:05

       DPNI1, DPNI3, e1000#0 [PRIME]

Warning: e1000#0 MAC addresses don't match:

Address in SROM is         00:15:17:8e:7e:05

Address in environment is  00:e0:0c:00:7a:02

=>

=> usb start

(Re)start USB...

USB0:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 0 for devices... 2 USB Device(s) found

USB1:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 1 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 1 Storage Device(s) found

=> usb reset

(Re)start USB...

USB0:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 0 for devices... 2 USB Device(s) found

USB1:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 1 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 1 Storage Device(s) found

=> usb tree

USB device tree:

  1  Hub (5 Gb/s, 0mA)

  |  u-boot XHCI Host Controller

  |

  +-2  Mass Storage (5 Gb/s, 224mA)

       SanDisk Ultra Fit 4C531123641015104115

    

  3  Hub (5 Gb/s, 0mA)

     u-boot XHCI Host Controller

  

=> usb info

1: Hub,  USB Revision 3.0

- u-boot XHCI Host Controller

- Class: Hub

- PacketSize: 9  Configurations: 1

- Vendor: 0x0000  Product 0x0000 Version 1.0

   Configuration: 1

   - Interfaces: 1 Self Powered 0mA

     Interface: 0

     - Alternate Setting 0, Endpoints: 1

     - Class Hub

     - Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms

2: Mass Storage,  USB Revision 3.0

- SanDisk Ultra Fit 4C531123641015104115

- Class: (from Interface) Mass Storage

- PacketSize: 9  Configurations: 1

- Vendor: 0x0781  Product 0x5583 Version 1.0

   Configuration: 1

   - Interfaces: 1 Bus Powered 224mA

     Interface: 0

     - Alternate Setting 0, Endpoints: 2

     - Class Mass Storage, Transp. SCSI, Bulk only

     - Endpoint 1 In Bulk MaxPacket 1024

     - Endpoint 2 Out Bulk MaxPacket 1024

3: Hub,  USB Revision 3.0

- u-boot XHCI Host Controller

- Class: Hub

- PacketSize: 9  Configurations: 1

- Vendor: 0x0000  Product 0x0000 Version 1.0

   Configuration: 1

   - Interfaces: 1 Self Powered 0mA

     Interface: 0

     - Alternate Setting 0, Endpoints: 1

     - Class Hub

     - Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms

=> usb storage

  Device 0: Vendor: SanDisk Rev: 1.00 Prod: Ultra Fit

            Type: Removable Hard Disk

            Capacity: 30550.0 MB = 29.8 GB (62566488 x 512)

=> usb dev

USB device 0: Vendor: SanDisk Rev: 1.00 Prod: Ultra Fit

            Type: Removable Hard Disk

            Capacity: 30550.0 MB = 29.8 GB (62566488 x 512)

=> usb write a0000000 0 800

USB write: device 0 block # 0, count 2048 ... 2048 blocks write: OK

=> usb read b0000000 0 800

USB read: device 0 block # 0, count 2048 ... 2048 blocks read: OK

=> cmp.b a0000000 b0000000 100000

Total of 1048576 byte(s) were the same

=>

The attached is the Linux Kernel log.

If your problem remains, would you please also provide your u-boot log?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
1,567 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Anandha Kumar M,

USB 3.0 is supported since 20150515 release.

There are two USB ports on LS2085QDS, please use USB1 to do USB 3.0 verification.

About RCW, please refer to field RCW[USB] and RCW[USB3_CLK_FSEL], the default RCW provided in the SDK ISO is fine.

The following is USB 3.0 test log in u-boot with SanDisk USB 3.0 storage device.

U-Boot 2015.01Layerscape2-SDK+g551206e (Apr 04 2015 - 14:20:34)

SoC:  LS2085E (0x87010010)

Clock Configuration:

       CPU0(A57):1600 MHz  CPU1(A57):1600 MHz  CPU2(A57):1600 MHz 

       CPU3(A57):1600 MHz  CPU4(A57):1600 MHz  CPU5(A57):1600 MHz 

       CPU6(A57):1600 MHz  CPU7(A57):1600 MHz 

       Bus:      600  MHz  DDR:      1333.333 MHz     DP-DDR:   1333.333 MHz

Reset Configuration Word (RCW):

       00: 40282830 40400040 00000000 00000000

       10: 00000000 00200000 00200000 00000000

       20: 00c12980 00002580 00000000 00000000

       30: 00000e0b 00000000 00000000 00000000

       40: 00000000 00000000 00000000 00000000

       50: 00000000 00000000 00000000 00000000

       60: 00000000 00000000 00027000 00000000

       70: 492a0000 00000000 00000000 00000000

Board: LS2085E-QDS, Board Arch: V1, Board version: B, boot from vBank: 4

FPGA: v7 (LS2085AQDS_2015_0407_1232), build 169 on Tue Apr 07 16:32:55 2015

SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz

SERDES2 Reference : Clock1 = 100 separate SSCGMHz Clock2 = 100 separate SSCGMHz

I2C:   ready

DRAM:  Initializing DDR....using SPD

Detected UDIMM 18ASF1G72AZ-2G1A1

Detected UDIMM 18ASF1G72AZ-2G1A1

DP-DDR:  Detected UDIMM 18ASF1G72AZ-2G1A1

19.5 GiB

DDR    15.5 GiB (DDR4, 64-bit, CL=9, ECC on)

       DDR Controller Interleaving Mode: 256B

       DDR Chip-Select Interleaving Mode: CS0+CS1

DP-DDR 4 GiB (DDR4, 32-bit, CL=9, ECC on)

       DDR Chip-Select Interleaving Mode: CS0+CS1

Waking secondary cores to start from fff18000

All (8) cores are up.

Using SERDES1 Protocol: 42 (0x2a)

Using SERDES2 Protocol: 73 (0x49)

Flash: 128 MiB

NAND:  512 MiB

MMC:   FSL_SDHC: 0

EEPROM: NXID v1

PCIe1: disabled

PCIe2: disabled

PCIe3: disabled

PCIe4: Root Complex x1 gen1, regs @ 0x3700000

     01:00.0    - 8086:107d - Network controller

PCIe4: Bus 00 - 01

In:    serial

Out:   serial

Err:   serial

Target spinup took 0 ms.

AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst

Found 1 device(s).

SCSI:  Net:   qds: WRIOP: Supported SerDes Protocol 0x2a

qds: WRIOP: Supported SerDes Protocol 0x49

mdio_register: non unique device name 'FSL_MDIO1'

Phy 28 not found

PHY reset timed out

Phy 29 not found

PHY reset timed out

Phy 30 not found

PHY reset timed out

Phy 31 not found

PHY reset timed out

crc32+

fsl-mc: Booting Management Complex ... SUCCESS

fsl-mc: Management Complex booted (version: 6.0.4, boot status: 0x1)

fsl-mc: Deploying data path layout ... SUCCESS

e1000: 00:15:17:8e:7e:05

       DPNI1, DPNI3, e1000#0 [PRIME]

Warning: e1000#0 MAC addresses don't match:

Address in SROM is         00:15:17:8e:7e:05

Address in environment is  00:e0:0c:00:7a:02

=>

=> usb start

(Re)start USB...

USB0:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 0 for devices... 2 USB Device(s) found

USB1:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 1 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 1 Storage Device(s) found

=> usb reset

(Re)start USB...

USB0:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 0 for devices... 2 USB Device(s) found

USB1:   Register 200017f NbrPorts 2

Starting the controller

USB XHCI 1.00

scanning bus 1 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 1 Storage Device(s) found

=> usb tree

USB device tree:

  1  Hub (5 Gb/s, 0mA)

  |  u-boot XHCI Host Controller

  |

  +-2  Mass Storage (5 Gb/s, 224mA)

       SanDisk Ultra Fit 4C531123641015104115

    

  3  Hub (5 Gb/s, 0mA)

     u-boot XHCI Host Controller

  

=> usb info

1: Hub,  USB Revision 3.0

- u-boot XHCI Host Controller

- Class: Hub

- PacketSize: 9  Configurations: 1

- Vendor: 0x0000  Product 0x0000 Version 1.0

   Configuration: 1

   - Interfaces: 1 Self Powered 0mA

     Interface: 0

     - Alternate Setting 0, Endpoints: 1

     - Class Hub

     - Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms

2: Mass Storage,  USB Revision 3.0

- SanDisk Ultra Fit 4C531123641015104115

- Class: (from Interface) Mass Storage

- PacketSize: 9  Configurations: 1

- Vendor: 0x0781  Product 0x5583 Version 1.0

   Configuration: 1

   - Interfaces: 1 Bus Powered 224mA

     Interface: 0

     - Alternate Setting 0, Endpoints: 2

     - Class Mass Storage, Transp. SCSI, Bulk only

     - Endpoint 1 In Bulk MaxPacket 1024

     - Endpoint 2 Out Bulk MaxPacket 1024

3: Hub,  USB Revision 3.0

- u-boot XHCI Host Controller

- Class: Hub

- PacketSize: 9  Configurations: 1

- Vendor: 0x0000  Product 0x0000 Version 1.0

   Configuration: 1

   - Interfaces: 1 Self Powered 0mA

     Interface: 0

     - Alternate Setting 0, Endpoints: 1

     - Class Hub

     - Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms

=> usb storage

  Device 0: Vendor: SanDisk Rev: 1.00 Prod: Ultra Fit

            Type: Removable Hard Disk

            Capacity: 30550.0 MB = 29.8 GB (62566488 x 512)

=> usb dev

USB device 0: Vendor: SanDisk Rev: 1.00 Prod: Ultra Fit

            Type: Removable Hard Disk

            Capacity: 30550.0 MB = 29.8 GB (62566488 x 512)

=> usb write a0000000 0 800

USB write: device 0 block # 0, count 2048 ... 2048 blocks write: OK

=> usb read b0000000 0 800

USB read: device 0 block # 0, count 2048 ... 2048 blocks read: OK

=> cmp.b a0000000 b0000000 100000

Total of 1048576 byte(s) were the same

=>

The attached is the Linux Kernel log.

If your problem remains, would you please also provide your u-boot log?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,566 Views
anandhakumarm
Contributor III

Hi Yiping,

Can u please provide the uboot image u have used for this usb testing ? so that i will also use the same uboot and test the same..

Thanks

Anandh..

0 Kudos
1,566 Views
anandhakumarm
Contributor III

Hi Yiping,

Actually we have the same settings in RCW[USB] and RCW[USB3_CLK_FSEL]. I didnt change that one, Anyway i will check one more time and update u..

--

Thanks

Anandh

0 Kudos