iMX6 Quad doesn't boot after External Reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Quad doesn't boot after External Reset

Jump to solution
1,618 Views
tamilarasane
Contributor III

In Imx6 Quad , after pressing RESET switch SOM doesn't boot again. it boots only after hard power on/off.

As per my understanding, through external reset released, internal Reset will release only after  VDD_ARM_CAP and VDD_SOC_CAP supplies
are stable (internal  LDO_CORE and LDO_SOC).

so , i doubt these internal voltage domains and their input voltages  VCC_SW1AB_CORE and VCC_SW1C_SOC of PMIC (MMPF0100F0AEP)

Findings:

1. in Linux, boots  after reset  switch is pressed with out problem and  VCC_SW1AB_CORE and VCC_SW1C_SOC voltages of  PMIC are fine. ( no voltage dip occurs-here current consumption from  VCC_SW1AB_CORE is  < 500mA)

2. In android
         1. if reset switch is pressed at the time of uboot, and kernel loading , booting occurs without problem ( up to this process current consumption form VCC_SW1AB_CORE is  < 700mA )
         2. once android application launches , current consumption from VCC_SW1AB_CORE is increased >900mA, and voltages dip occurs ( snap shot attached) if reset switch is pressed now,  doesn't boot again.


3. first dip occurs from 1.35 to 1.28V at that time current is around 700mA.  if i press reset switch here, boot occurs without problem

tek00012.bmp



4. After some time (  launching android application) continuous dip occurs  from ( 1.28V to 0.992V) here current is around 900mA  . if i reset here, board doesn't boot . and
VCC_SW1AB_CORE is in 0.992V itself.
tek00011.bmp
Green -VCC_SW1AB_CORE of PMIC
Blue-
VCC_SW1C_SOC of PMIC

Same issues occurs in 3 boards.

Is anyone faced this issue...? Pls let me know the solution for this.?

Thanks

Tamilarasan.

0 Kudos
1 Solution
1,150 Views
igorpadykov
NXP Employee
NXP Employee

HI Tamilarasan

recommended to use such reset circuit , which resets both PMIC and

i.MX6, because for example, if i.MX6 in ldo-bypas mode, resetting only

processor will hang it (PMIC voltages may be insufficient for successful boot).

This is addressed by Sabre SD reset circuit design (WDOG connection to PWRON)

i.MX6_SABRE_SDP_DESIGNFILES  spf-27392 p.21 and description in Release Notes

Release Notes.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
1,151 Views
igorpadykov
NXP Employee
NXP Employee

HI Tamilarasan

recommended to use such reset circuit , which resets both PMIC and

i.MX6, because for example, if i.MX6 in ldo-bypas mode, resetting only

processor will hang it (PMIC voltages may be insufficient for successful boot).

This is addressed by Sabre SD reset circuit design (WDOG connection to PWRON)

i.MX6_SABRE_SDP_DESIGNFILES  spf-27392 p.21 and description in Release Notes

Release Notes.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,150 Views
tamilarasane
Contributor III

HI igor,

yes your are correct, this issues occurs only at the time of LDO By pass mode..

can you pls share the errata and workarounds for imx6..? where i will get..?

Thanks,

Tamilarasan

0 Kudos
1,150 Views
igorpadykov
NXP Employee
NXP Employee

HI Tamilarasan

this is not erratum, this is expected behaviour,

workaround is given in my previous answer.

~igor

0 Kudos
1,150 Views
tamilarasane
Contributor III

hi igor,

can you pls share the  "spf-27392 p.21 " document. i can't able to search..

Thanks,

Tamilarasan

0 Kudos
1,150 Views
igorpadykov
NXP Employee
NXP Employee

attached

~igor

0 Kudos