uboot ldo_bypass

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot ldo_bypass

2,193 Views
强王
Contributor IV

uboot:2014

kernel:3.10.53

 

 

UBOOT LOG:

 

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:  serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

mmc1 is current device

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

5545424 bytes read in 257 ms (20.6 MiB/s)

Booting from mmc ...

reading imx6q-sabresd.dtb

49575 bytes read in 18 ms (2.6 MiB/s)

Kernel image @ 0x12000000 [ 0x000000 - 0x549dd0 ]

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800f1a6

switch to ldo_bypass mode!

(这里的ldo_bypass作用是什么,并且还是用到了i2c,

如果我把UBOOT里的设置ldo_bypass删除,可以正常引导内核,内核会卡在Galcore version 5.0.11.25762这句话)

 

 

附件是正常的log

Original Attachment has been moved to: normallog.zip

Labels (1)
0 Kudos
1 Reply

508 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

are you able to boot with ldo enabled - using xxx-imx6q-sabresd-ldo.dtb ?

If yes - then probably you are having PMIC problems - please check

that it can be controlled by processor.

If not - then probably you have ddr errors and one needs to run DDR test

https://community.freescale.com/docs/DOC-96412

and update memory settings. Recommended to use FSL BSP

L3.10.53_1.1.0_iMX6QDLS_Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos