temperature sensor precision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

temperature sensor precision

541件の閲覧回数
leeyoungmoon
Contributor I

Hi,

I am using sabre lite from boundary device with iMX6 quad.

the temperature reading is only integer value,

is iMX6 capable of better precision at the first place?

I just wonder it just removed in calibration process?

thanks in advance

ラベル(1)
0 件の賞賛
2 返答(返信)

405件の閲覧回数
Yuri
NXP Employee
NXP Employee

The temperature sensor is not high precision device.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

405件の閲覧回数
leeyoungmoon
Contributor I

At least, we can estimate the trend helpful than a degree step.

though iMX6 reads temperature millicelcius, sabrelite truncates temperature precision,

is the measurement that unreliable? can't we even estimate the trend at worst?

0 件の賞賛