Hello, I have a target board with a MC9S12XEP100 chip. The flash of the MCU chip is un-protected and un-secured. I want to get the machine code file or assembly file (*.abs, or *.s19). What should I do?
PS: I have succesfully connected the target board using the BDM (P&E USB Multilink Inerface) via the software - hiwave.exe, and see the contents of the Flash memory, as well as the Assemble codes in the Windows of "Memory" and "Assemble" of the hiwave.exe software, respectively. But I don't know how to save them as a *.abs file or a *.s19 file. The copy command cannot be used in the Windows "Memory" or "Assemble" of the hiwave.exe software
hello Kun,
my colleague already provided the answer:
How to get the machine code file from a target board with an un-protected or un-secured Flash MCU?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Jennie, thanks for digging that out :-)
you are welcome!
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------