bsp:linux3.0.35 cpu:imx6q.
I need to use opengl and gles.To use multiple-buffer rendering, I set 'export FB_MULTI_BUFFER=2'. I download the gpu_sdk_v1.00.gz, and execute the example in the file. That comes the problem. I stop the test app using 'ctrl+c', and then exectue a app of clear screen. Sometime, the screen woule be clear successfully. Sometimes, it had no effect. By the way, the app of clear screen always success before I set 'export FB_MULTI_BUFFER=2'. How can I make my display app always effect on the screen when export FB_MULTI_BUFFER=2?
Hi jie,
To specify the display device, use the environment variable FB_FRAMEBUFFER_n, where n = any positive
integer. Example usage syntax:
export FB_FRAMEBUFFER_0=/dev/fb0
export FB_FRAMEBUFFER_1=/dev/fb1
export FB_FRAMEBUFFER_2=/dev/fb2
To open a specific framebuffer device, set environment variables to their proper values (e.g., set
FB_FRAMEBUFFER_0 = /dev/fb0). If there are no environment variables set, the driver will try to use the
default fb devices (fb0 for index 0, fb1 for index 1, fb2 for index 2).
Hope this helps