Debugging KV3 with USBDM: Has USBDM support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging KV3 with USBDM: Has USBDM support?

537 Views
fabio_vila
Contributor I

I'm attempting debug Kinetis MKV3 with USBDM+FRDM-KL25Z. The FRDM with USBDM works great. However when connected on Kinetis KV3 there is no option to select this MCU in ARM_GDBServer. The autodetect button fails too:

"

Failed to probe target

Reason: Execution of TCL script returned an error

"

EDIT:

In GDB Settings / ARM_GDBServer the list box don't have any KV3 MCU.

Captura de tela de 2015-04-03 09_58_27.png

Mensagem editada por: fabio ... Hi, Screenshot added to the text.

0 Kudos
2 Replies

375 Views
pgo
Senior Contributor V

Hi Zhang,

Sorry USBDM does not have support for KV devices.

It is likely that it will be added in a future version  but at the moment I don;t have any KV devices to test with.

bye

375 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi fabio,

can you please specify what is "no option to select this MCU" with screenshot?

if you use KDS, please see below for how to use USBDM in KDS2.0

USBDM in KDS 2.0


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos