Hello
I'm trying to bitbake a Core-image-minimal with yocto daisy(for an imx28evk board).
But I've a compilation error :
ERROR: Function failed: do_compile (log file is located at /home/gwio/fsl-community-bsp/build/tmp/work/x86_64-linux/perl-native/5.14.3-r0/temp/log.do_compile.17607)
ERROR: Logfile of failure stored in: /home/gwio/fsl-community-bsp/build/tmp/work/x86_64-linux/perl-native/5.14.3-r0/temp/log.do_compile.17607
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 12 -e MAKEFLAGS=
| `sh cflags "optimize='-O2'" doio.o` -fPIC doio.c
| gcc -o generate_uudmap -L/home/gwio/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/lib -L/home/gwio/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/lib -Wl,-rpath-link,/home/gwio/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/lib -Wl,-rpath-link,/home/gwio/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/lib -Wl,-rpath,/home/gwio/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/lib -Wl,-rpath,/home/gwio/fsl-community-bsp/build/tmp/sysroots/x86_64-linux/lib -Wl,-O1 generate_uudmap.o -lnsl -ldl -lm -lcrypt -lutil -lpthread -lc
| ./generate_uudmap uudmap.h bitcount.h
| `sh cflags "optimize='-O2'" globals.o` -fPIC globals.c
| CCCMD = gcc -DPERL_CORE -c -D_REENTRANT -D_GNU_SOURCE -fno-strict-aliasing -pipe -fstack-protector -I/usr/local/include -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64 -std=c89 -O2 -Wall -ansi -W -Wextra -Wdeclaration-after-statement -Wendif-labels -Wc++-compat -Wwrite-strings
| CCCMD = gcc -DPERL_CORE -c -D_REENTRANT -D_GNU_SOURCE -fno-strict-aliasing -pipe -fstack-protector -I/usr/local/include -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64 -std=c89 -O2 -Wall -ansi -W -Wextra -Wdeclaration-after-statement -Wendif-labels -Wc++-compat -Wwrite-strings
| doio.c:39:20: error: conflicting types for 'shmat'
| extern Shmat_t shmat (int, char *, int);
| ^
| In file included from doio.c:37:0:
| /usr/include/x86_64-linux-gnu/sys/shm.h:56:14: note: previous declaration of 'shmat' was here
| extern void *shmat (int __shmid, const void *__shmaddr, int __shmflg)
| ^
| doio.c: In function 'Perl_nextargv':
| doio.c:871:7: warning: ignoring return value of 'fchown', declared with attribute warn_unused_result [-Wunused-result]
| (void)fchown(PL_lastfd,fileuid,filegid);
| ^
| In file included from perl.h:3395:0,
| from doio.c:27:
| doio.c: In function 'S_exec_failed':
| iperlsys.h:769:39: warning: ignoring return value of 'write', declared with attribute warn_unused_result [-Wunused-result]
| #define PerlLIO_write(fd, buf, count) write((fd), (buf), (count))
| ^
| doio.c:1383:2: note: in expansion of macro 'PerlLIO_write'
| PerlLIO_write(fd, (void*)&e, sizeof(int));
| ^
| makefile:248: recipe for target 'doio.o' failed
| make: *** [doio.o] Error 1
| make: *** Waiting for unfinished jobs....
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/gwio/fsl-community-bsp/build/tmp/work/x86_64-linux/perl-native/5.14.3-r0/temp/log.do_compile.17607)
ERROR: Task 694 (/home/gwio/fsl-community-bsp/sources/poky/meta/recipes-devtools/perl/perl-native_5.14.3.bb, do_compile) failed with exit code '1'
WARNING: Failed to fetch URL ftp://ftp.uni-erlangen.de/pub/Linux/LOCAL/dosfstools/dosfstools-2.11.src.tar.gz, attempting MIRRORS if available
NOTE: Tasks Summary: Attempted 720 tasks of which 703 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Can you help me ?
Solved! Go to Solution.
I think I found the solution by myself.
I edited sys/shm.h and I added : "#define HAS_SHMAT_PROTOTYPE".
In this case, doio.c will not try to redefined SHMAT prototype and perl compiles with no error.
I think I found the solution by myself.
I edited sys/shm.h and I added : "#define HAS_SHMAT_PROTOTYPE".
In this case, doio.c will not try to redefined SHMAT prototype and perl compiles with no error.