KL04 Hard Fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL04 Hard Fault

597 Views
sergigomis
Contributor III

Hi.

I have problems with KL04Z8.

When I try to debug a simple aplication  (One BitIO toogle for example), I can't debug because inmmediatly appears a PS_ISR(Cpu_ivINT_Hard_Fault).

I use a Kinetis Design Studio 1.1.1

I need do special something with CPU configuration ??

Thank's

Sergi

Tags (3)
0 Kudos
1 Reply

361 Views
adriancano
NXP Employee
NXP Employee

Hi,

This issue was already discussed, check this thread:

https://community.freescale.com/message/436064#436064

:smileyinfo: Remember posting your questions in a dedicated space, for example Kinetis Design Studio there it will have more visibility.

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos