imx6dl HDMI can't support 1024x768

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dl HDMI can't support 1024x768

3,684 Views
tanxiaofei
Contributor I

Our application of scene must use 1024x768 for HDMI. But i

found that imx6dl's HDMI transmitter have a problem to output in

1024x768. Others is ok, such as 1280x1024, 800x600.

So, does the imx6dl HDMI support 1024x768 output? 

board: Ours

cpu: IMX6DL

BSP: L3.0.35_4.1.0_130816_source.tar.gz

Labels (2)
0 Kudos
Reply
6 Replies

2,150 Views
PeterChan
NXP Employee
NXP Employee

Hi Xiaofei,

Would you please try the attached patch? Please change the HDMI resolution to 1024x768 in your kernel command line.

Thanks,

Peter

2,150 Views
tanxiaofei
Contributor I

Hi Peterchan,

Thank you. The issue has been fixed. Our display device doesn't support 1024x768.

So, it will be ok to add an default timing for 1024x768 to mode list after got HDMI edid.

0 Kudos
Reply

2,150 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi xiaofei,

If your problem have solved, would you please help close this thread by clicking the Correct Answer or Helpful Answer button. Thanks a lot.
Have a great day

Best Regards

Dan

0 Kudos
Reply

2,150 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Xiaofei,

You can refer to the thread iMX6 HDMI output 1366x768 resolution.
Have a great day,

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,150 Views
OtavioSalvador
Senior Contributor II

The kernel restricts it, if I recall correctly.

You can take a look in Boundary Devices' kernel tree as they have a patch to address it and base on that.

0 Kudos
Reply

2,150 Views
tanxiaofei
Contributor I

Hi Otavio,

Thank you very much. I don't know how to get kernel tree or patch from Boundary Devices. Could you show me?

Best wishes,

Xiaofei

0 Kudos
Reply