Hi,
I'm not new to embedded linux but I'm a newbie to OpenGl programming.
I would like to compile a Simple OpenGl program to be able to run on an iMX6Q board (running linux: framebuffer build).
Can anyone give me links from where I can start?
I have the following questions:
1) Do I need Vivante dev libraries on the Ubuntu Host PC to cross compile?
My understanding is that as OpenGl is a standard I only need header files, GPU specific libraries are not needed (at least for dynamic linking). Am I correct?
2) Does the Vivante VDK/VTK released by Freescale allows cross compiling?
Any inputs will be of help to me.
-Pj
Hi Prasant
"yes", on both questions, for starting
please look at below presentations
Freescale FTF Americas 2014 - Vivante GPU Highlights
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------