Hi,
We are designing a product using p2020cpu refering to the design of p2020rdb-pc,booting from NOR. We use the u-boot of p1_p2_rdb_pc. It can work.
Now I want to modify the NOR's base address to 0x4f000000. So I modify the following codes in p1_p2_rdb_pc.h :
#define CONFIG_SYS_TEXT_BASE | 0xeff80000 |
#define CONFIG_RESET_VECTOR_ADDRESS | 0xeffffffc |
#define CONFIG_SYS_FLASH_BASE | 0xef000000 |
But then the board can't work. It's blank in minicom.
Where am I wrong?
Best regards,
Min Zhao
Solved! Go to Solution.
Is the physical address of NOR Flash is 0x4f000000?
In the original memory map of p1_p2_rdb_pc, 0x4f000000 should be DDR.
Have a great day,
Yiping Wang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear All,
I have P2020-rdb board and also have codewarrior TAP and IDE.
Please let me know i can have u-boot, uImage and file system in NOR flash, how i can do tftpboot or NFS boot.
Please provide good document or link so that i can flash and boot the board easily.
Thanks,
VP
Did you unset CONFIG_PHYS_64BIT?
Yes,I don't make 36-bit.
Best regards,
Min Zhao
Is the physical address of NOR Flash is 0x4f000000?
In the original memory map of p1_p2_rdb_pc, 0x4f000000 should be DDR.
Have a great day,
Yiping Wang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------