Hii all,
I have problem to download Code onto the MPC555 either on
RAM or Flash using CodeWarrior.
CodeWarrior version 8.7 and my PC is XP 2002 SP3.
when trying to download the Hello project on RAM I got this
error. >> *pic (ram_error)*.
and when trying to set the Flash setting, then need to erase step(from
manual), I couldn't get connect to MPC555 and I have error but without
description; as in the *pic (flash_error)*.
Also when trying to download Code onto MPC555 using MATLAB via Serial
ports, I have this error; *pic (com_error)*.
Note here that I have used the serial ports and got successful downloading
before many times, BUT suddenly it isn't able to download and always give
the Com error, although I haven't change any thing to the
port,configurations and jumper setting.
Don't know why!
Please, any help toward this urgent problem?
Regards,
Do you figure out this problem?
I also face this problem too. If you have some sultion to this problem.
Could you let me know? I am very please if you can answer me through board or through my email: yeqin.wang@ttu.edu.
Thanks,
yeqin