At /drivers/video/mxc/mxc_edid.c,
const struct fb_videomode mxc_cea_mode[64] = {
/* #1: 640x480p@59.94/60Hz 4:3 */
[1] = {
NULL, 60, 640, 480, 39722, 48, 16, 33, 10, 96, 2, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, 0,
},
/* #2: 720x480p@59.94/60Hz 4:3 */
[2] = {
NULL, 60, 720, 480, 37037, 60, 16, 30, 9, 62, 6, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, 0,
},
/* #3: 720x480p@59.94/60Hz 16:9 */
[3] = {
NULL, 60, 720, 480, 37037, 60, 16, 30, 9, 62, 6, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #4: 1280x720p@59.94/60Hz 16:9 */
[4] = {
NULL, 60, 1280, 720, 13468, 220, 110, 20, 5, 40, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0
},
/* #5: 1920x1080i@59.94/60Hz 16:9 */
[5] = {
NULL, 60, 1920, 1080, 13763, 148, 88, 15, 2, 44, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_INTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #6: 720(1440)x480iH@59.94/60Hz 4:3 */
[6] = {
NULL, 60, 1440, 480, 18554/*37108*/, 114, 38, 15, 4, 124, 3, 0,
FB_VMODE_INTERLACED | FB_VMODE_ASPECT_4_3, 0,
},
/* #7: 720(1440)x480iH@59.94/60Hz 16:9 */
[7] = {
NULL, 60, 1440, 480, 18554/*37108*/, 114, 38, 15, 4, 124, 3, 0,
FB_VMODE_INTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #8: 720(1440)x240pH@59.94/60Hz 4:3 */
[8] = {
NULL, 60, 1440, 240, 18554, 114, 38, 16, 4, 124, 3, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #9: 720(1440)x240pH@59.94/60Hz 16:9 */
[9] = {
NULL, 60, 1440, 240, 18554, 114, 38, 16, 4, 124, 3, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #16: 1920x1080p@60Hz 16:9 */
[16] = {
NULL, 60, 1920, 1080, 6734, 148, 88, 36, 4, 44, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #17: 720x576pH@50Hz 4:3 */
[17] = {
NULL, 50, 720, 576, 37037, 68, 12, 39, 5, 64, 5, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, 0,
},
/* #18: 720x576pH@50Hz 16:9 */
[18] = {
NULL, 50, 720, 576, 37037, 68, 12, 39, 5, 64, 5, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #19: 1280x720p@50Hz */
[19] = {
NULL, 50, 1280, 720, 13468, 220, 440, 20, 5, 40, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #20: 1920x1080i@50Hz */
[20] = {
NULL, 50, 1920, 1080, 13480, 148, 528, 15, 5, 528, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_INTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #31: 1920x1080p@50Hz */
[31] = {
NULL, 50, 1920, 1080, 6734, 148, 528, 36, 4, 44, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #32: 1920x1080p@23.98/24Hz */
[32] = {
NULL, 24, 1920, 1080, 13468, 148, 638, 36, 4, 44, 5,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_16_9, 0,
},
/* #35: (2880)x480p4x@59.94/60Hz */
[35] = {
NULL, 60, 2880, 480, 9250, 240, 64, 30, 9, 248, 6, 0,
FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, 0,
};
my hdmi display monitor have 20 mode, but it only match the first item in mxc_cea_mode, so at last, my hdmi only work on 640*480.
the array can add other mode by myself?
Hi Zhiyan,
You can't simply add CEA modes, because they are tied to audio output.
You can over-ride the requirement for CEA modes as we've done in our
kernels, but this will mess up the audio clocking.
See these two posts for more details:
Hi Eric:
Thank you for your advice.
I try the method. But my monitor does not light at 1024*768. It only work at 640*480.
There are other problems. My first monitor is vga, it use ipu0 and di0, it works at 1024*768@60 video mode, its name is DISP3 BG;
my second monitor is hdmi, it use ipu1 and di0, it works at 640*480@60 video mode, its name is DISP4 BG.
Each monitor use one ipu, i.MX6q should support?
Could you give me some more hits?
Hi Zhiyan,
i.MX6Q definitely supports this, and you should get proper audio with VGA timings (because that's a CEA mode).
Are you operating with EDID support?
Hi Eric:
My HDMI monitor adopt edid, and My VGA monitor also adopt edid such as dvi.
I will try again.
Thanks!