Which pins of KL25z are connected with Accelrometer MM8451Q ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which pins of KL25z are connected with Accelrometer MM8451Q ?

Jump to solution
682 Views
amanmunjal
Contributor I

I m planning to make a project with inbuilt Accelerometer on the Free Scale KL25Z board so i wanted to know which pins are connected with with of output bus is connected with accelerometer .

Labels (1)
0 Kudos
1 Solution
436 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi aman,

You can refer the Schematics of FRDM-KL25Z board.

You can find the Schematics of FRDM-KL25Z (RevE) in FRDM-KL25Z_SCH_REV_E.

See below:

MMA8451.jpg

SCL SDA.jpg

INT.jpg

Also you can find the Schematics of RevD FRDM-KL25Z_SCH_REV_D

Hope that help

Best Regards

Robin

View solution in original post

0 Kudos
3 Replies
436 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Aman,

You might also find useful my example code for the MMA8451Q accelerometer and FRDM-KL25Z platform.

Regards,

Tomas

0 Kudos
437 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi aman,

You can refer the Schematics of FRDM-KL25Z board.

You can find the Schematics of FRDM-KL25Z (RevE) in FRDM-KL25Z_SCH_REV_E.

See below:

MMA8451.jpg

SCL SDA.jpg

INT.jpg

Also you can find the Schematics of RevD FRDM-KL25Z_SCH_REV_D

Hope that help

Best Regards

Robin

0 Kudos
436 Views
BlackNight
NXP Employee
NXP Employee

Hello,

I recommend to have a look at the schematics: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z

(check with revision of board you have, either E or D)

Otherwise have a look here: http://mcuoneclipse.com/2012/09/21/tutorial-accelerating-the-kl25z-freedom-board/