I do not understand the nandflash(mt29f2g16aad) after power is how to start?when i download the firmware to the nandflash mt29f2g16aad from codewarrior10.1, the download tip in the cw10.1 is in the following statement.
******************************************************************************
Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Elf Format.
Downloading 0x00000F80 bytes to be programmed at 0x00000000
Programming ....
Program Command Succeeded
Downloading 0x0001403C bytes to be programmed at 0x00000F80
Programming ....
Program Command Succeeded
cmdwin::fl::verify
-------------------------
Verifying file D:\Freesacleworkspace\2\twrmcf54418_Ext_Flash_Debug\2.elf
Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Elf Format.
Downloading 0x00000C6E at address 0x40004020
Writing verify function code
Running ...
Reading verify status
Downloading 0x00010000 at address 0x40004020
Writing verify function code
Running ...
Reading verify status
Downloading 0x0000403C at address 0x40004020
Writing verify function code
Running ...
Reading verify status
Verify Command Succeeded
******************************************************************************
I do not understand what is the address of the store from 0x00000000 to 0x00000F7F and from 0x00000F80 to (0x00000F80+0x0001403C-1).is it a boot?where can i find it in the cw10.1?
and is it my firmware at address 0x40004020?Who can help me? thanks!