I have a problem with the Flash programmer of CW, when I try to write the internal flash an error happen (below here there is the log information), if I use a third part CFFLasher all work correctly, have someone an idea of this problem??
In the flash programmer I load the CFM_MCF52235.xlm setting.
Thanks in advance.
Regards
Domenico
======================================================================
=== Execute: Program
=== Timestamp: Tue Jul 31 17:15:57 2007
=== Flash Device: CFM_MCF52235
=== Flash Organization: 8Kx32x1
=== Flash Mem Start Addr: 0x00000000
=== Flash Mem End Addr: 0x0003FFFF
======================================================================
Using Algorithm: CFM_MCFCOMMON.elf
Loading Flash Device Driver at: 0x20000000
Flash Driver Buffer is at: 0x20001FB0
Flash Driver Buffer Size is: 0x00006050
Done
Initialization Command Succeeded
System clock: 25000KHz
Programming file C:\Test Motorola\52235EVB\52235EVB\bin\M52235EVB_INTERNAL_FLASH.elf
Trying auto-detect...
File is NOT of type Motorola S-Record Format.
Auto-detection is successful.
File is of type Elf Format.
Programming 0x00000418 bytes of Target Memory at 0x00000000
Flash Programmer: Flash driver reports the following error(s): Chip reported error during program
Timestamp: Tue Jul 31 17:16:04 2007