Hi,
is there any IOMUX tool for the vybrid series?
Could you also confirm if the following mapping is correct?
UART0:
- SCI0-TX, RX, CTS, RTS
UART1:
- SCI1-TX, RX, CTS, RTS
UART2:
- SCI2-TX, RX, CTS, RTS
UART3:
- SCI3-TX, RX, CTS, RTS
UART4:
- SCI4-TX, RX, CTS, RTS
I found all of the above on ball pin mapping.
But, 19.8.2.2 of the reference manual is telling me differently?
Thanks
~RD
Solved! Go to Solution.
Dear R D,
if you dpwnload the reference manual from http://cache.freescale.com/files/32bit/doc/ref_manual/VYBRIDRM.pdf?fpsp=1&WT_TYPE=Reference%20Manual...
you will se two excel tables on the upper left hand corner of the pdf file. These are the IOMUX tools forr Vybrid series.
Mehmet Ali
Dear R D,
if you dpwnload the reference manual from http://cache.freescale.com/files/32bit/doc/ref_manual/VYBRIDRM.pdf?fpsp=1&WT_TYPE=Reference%20Manual...
you will se two excel tables on the upper left hand corner of the pdf file. These are the IOMUX tools forr Vybrid series.
Mehmet Ali