Bootloader and EEPROM NVMFlex with K20

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader and EEPROM NVMFlex with K20

461 Views
night
Contributor II

Hi,

I'm trying to use bootloader with EEProm over NVMFlex memory. The application works fine without the bootloader but when I work with bootloader I can't write on the EEPROM. I just enabled the Partitioning for device register on advanced options in the project menu. The code value used with this is 3303 (for use 2KB eeprom). With the bootloader project I use the same configuration but it doesn't work. Where is the problem?

Thank you and sorry for my English.

Best Regards,

          Miguel Ángel.

Labels (1)
0 Kudos
1 Reply

294 Views
vfilip
NXP Employee
NXP Employee

Hello,

we would need more deatils about the bootloader. Could you please provide more details of the project or in the best case some project how to reproduce it?

best regards

Vojtech Filip

Processor Expert Support Team

0 Kudos