imx-ipuv3 imx-ipuv3.0: IPU Warning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-ipuv3 imx-ipuv3.0: IPU Warning

2,438 Views
Raana
Contributor III

Hi,

Currently I am working on imx6 Dual lite/solo (i.MX6Q/D/S) SabreSD based custom board

I tried to run the HDMI video (2.2min HD video). while, running the video below prints or coming on the console

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x08800000

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000

whenever the prints is coming the video is going off. After some fraction of seconds it'll come again.

what is the issue ??

How to recover it ??

Thanks in Advance.

Regards, J.P.Raja


Labels (1)
0 Kudos
1 Reply

598 Views
Yuri
NXP Employee
NXP Employee