the problem of User Guide for DDR Stress Tester Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the problem of User Guide for DDR Stress Tester Kit

1,557 Views
zhangyinhua
Contributor I

I use the DDR Stress Tester Kit.

I can see :

mx53_p.png

in the "Please enter the number chip......"step

when I input the "0" to select 0 for CSD0 ,appear "Not a vaild number!"

and I can't continue.

???

Labels (1)
0 Kudos
3 Replies

615 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please try to type the command like this:

example:

DDR_Stress_Tester  –t  mx53  –df  MX53_TO2_DDR2_EVK_ARD.inc  –com 4

615 Views
yektaayduk
Contributor II

I'm running the DDR_test  on my custom mx53 board .

The consol output is below ,it waits forever without printing any result ?

C:\DDR_Stress>DDR_Stress_Tester -t mx53 -df MX53_DENETIM_DDR2_dene3.inc -com 1

HAB_TYPE: DEVELOP

Image loading...

download Image to IRAM OK

Running DDR test..., press "ESC" key to exit.


0 Kudos

615 Views
yektaayduk
Contributor II

Sorry the bin file was wrong ,now test is running and generating results:

C:\DDR_Stress>DDR_Stress_Tester -t mx53 -df MX53_DENETIM_DDR2_dene4.inc -com 1

HAB_TYPE: DEVELOP

Image loading...

download Image to IRAM OK

Running DDR test..., press "ESC" key to exit.

**************************************************************************

    DDR Stress Test (1.0) for MX53

    Build: Apr 13 2011, 13:44:13

    Freescale Semiconductor, Inc.

**************************************************************************

Please select the DDR density per chip select (in bytes) on the board

Type 0 for 128MB; 1 for 64MB; 2 for 32MB; 3 for 16MB

  DDR density selected (MB): 128

Please enter the number chip selects used on the board by the DDR

Type 1 for one chip select or 2 for two chip selects

Which chip select do you want to test, type 0 for CSD0 or 1 for CSD1

  You have chosen to to test CSD0 only

Would you like to run the DDR Stress Test (y/n)?

Run DDR stress test with incrementing DDR frequency (y/n)?

Enter 'y' to run with an incrementing DDR frequency

Enter 'n' to run at a static DDR frequency

Enter desired freq (125 to 400 MHz in steps of 5 MHz) to run test then hit enter

.

400MHz DDR clock will not increment

0

t0: memcpy11 SSN test

Address of bank1 failure: 0x71000000

Data was:                 0xaaaa

But pattern was:          0xffffffff

Source is wrong, it is: 0x40aa


0 Kudos