question about mx53 dual channel lvds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about mx53 dual channel lvds

925 Views
admin
Specialist II

I know mx53 have dual channel LVDS,can support two single lvds Interface Display,but my display use 17 inch Color TFT-LCD Module M170EG01 VH,The display supports the SXGA+ (1280(H) x 1024(V)) screen format and 16.7M colors (RGB 6-bits+Hi-RFC data).All input signals are 2 Channel LVDS interface ,and the interface need dual channel LVDS,The first LVDS port transmits odd pixels,while the second LVDS port transmits even pixels. So what can I do for it?

I know when use one lvds interface for display,For example I can set:

set bootargs_mmc setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcdi0fb:RGB666,XGA di0_primary ldb=di0 ip=none

  So,how can I set the param?

Labels (1)
0 Kudos
1 Reply

464 Views
nichosim
Contributor II

HEllo,

did you solved your problem With 17" display?

I'm working to the same configuration but i cannot have the display work properly in dualchannel...

0 Kudos