Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent

1,726 Views
harlenChen
Contributor I
We use the MC908QL4MDW.. But the logo on IC is MC908QL4MDW1? And sometimes, the logo is MC908QL4MDW2?  I want to konw the different??? I can not get the information about the '1' or '2' from the datasheet.
thx
Harlen
Labels (1)
0 Kudos
1 Reply

385 Views
RockyRoad
Contributor III
Harlan -
 
There was a problem with a mask set that the internal clock would not trim to the 25.6 MHz option. These parts are marked with the '1'.  Parts that will trim correctly at 25.6 MHz are marked with '2'.
 
If you are using an external crystal or if you are using the internal at 4, 8, or 12.8 MHz, then this won't make a difference.
 
- Rocky
0 Kudos