I have developed an application for MC56F8346 hybrid controller with CW7.0 with no problem. Later I've updated to CW7.3 to handle a brand new USB-TAP OnCE emulator, and the application stopped working properly.
Compiling it with CW7.0 everything works fine, while compiling *the same code* with CW7.3 it hangs... I found a different behaviour handling automatic variables. This code:
void dummy_function (void)
{ unsigned char array[3]={0x00, 0x01, 0x02};
if (array[0]==0x00&&array[1]==0x01&&array[2]==0x02)
printf("\nOk!");
else
printf("\nArray not init");
return;
}
returns "Ok" if compiled with rel 7.0, and "Array not init" with rel 7.3
Is this a bug? Someone reported a similar problem in thread "Defining a temporary array on stack". Quite funny!