Message Edited by imajeff on 04-21-200610:26 AM
Hi Alex,
we are using the a part of the flash i.e. 0x4000 to 0x41FF for storing some data base. so that the data is resided even after power re-cycle.
coming to the point, i'm not intending to say that when i do a power re-cycle, the flash is not getting updated. the problem that i'm facing is once i write data in to the flash in to the location that i have specified, when i read the data back, in some processors, one or two bytes are getting corrupted.
let me tell you in detail. what i have faced here in one of the processors is, when i write say some first 200 bytes with 1 to 200 and when i read back after writing, in one of the processors, the 86th byte was getting corrupted. in the sense i'm not getting 86 when i read... but i'm getting 32. in one more processor board, i got error reading the byte 182.
so, this behaviour is random. and if i have to suspect the code, the same code works fine in many of the processors.
please let me know if you want some more info.
Thanks,
Kalyan kumar P