i.MX Solutions Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Solutions Knowledge Base

Labels
  • General 294

Discussions

Sort by:
EM9280 with pins Added by Cheng Shi on June 15, 2012 at 2:09am This is an imx283 based board with 8 uart ports, 1 ethernet port, LCD interface, etc. It's size is smaller than that of a credit card.  
View full article
http://www.youtube.com/watch?v=qSUE8K53mrI&feature=player_embedded   Uploaded by Charbax on Jun 23, 2011 Discussion with Linaro employees about the status of ARM Powered laptops. Category: Science & Technology License: Standard YouTube License  
View full article
http://www.youtube.com/watch?feature=player_embedded&v=P1lycaQF6Nk   Uploaded by igalloway on Jul 21, 2011 Future Display Solutions Future Electronics Display Solutions Group is excited to re-launch the Future's Panel Interface Board (PIM). This is an enabler to help our customer designing Freescale I.MX and LCDs. With the Future's Panel Interface Module, customer can use Freescale i.MX evaluation kits to drive different displays of their choice for evaluation and prototyping.       We can provide full solutions for the customers including:   - Panel Interface Module (Free for qualified customers) - I.MX Evaluation Kits (EVK) - LCD Displays - Backlight Drivers - Cables Category: Science & Technology License: Standard YouTube License  
View full article
img-0004-fsl-ptx Added by Robert Schwebel on November 10, 2010 at 6:46pm   Bjoern Buerger from the Pengutronix team demonstrates a Qt 4.7 demo on the MX28.
View full article
http://www.youtube.com/watch?v=oR3VeeiKAOw&feature=player_embedded   Uploaded by BoundaryDevices on Feb 15, 2011 Dual Displays running in Portrait Mode on an IMX515 processor. Our NitrogenE board is connected to an HDMI monitor and a 7" 800x480 TTL display. OS is Debian. Category: Science & Technology License: Standard YouTube License  
View full article
Added by Johan Dams on June 24, 2010 at 7:07am   http://www.youtube.com/watch?feature=player_embedded&v=pOSluW6vHL8   Uploaded by Charbax on Jun 22, 2010 http://genesiamericas.com is presenting this awesome looking ARM Cortex A8 based Smartbook design, presented by Genesi who designed the hardware in collaboration with Pegatron of this latest generation of this Freescale Powered Smartbook design. For fun, we are running Microsoft Office through a high resolution version of Citrix viewer on the latest version of Ubuntu 10.4 for ARM processors. This could provide a one click online based software as a service solution. Want to run any X86 application on your ARM Laptop? Just click through the Citrix virtualization stuff and you can have it all running and smoothly. In theory, the apps could be processed by a grid and delivered much faster than on a single x86 processor based device.   Genesi are providing the hardware and software integration solution, in combination with Future Electronics, they can provide the whole solution to carriers, distributors, with the full bill of material, setting up the manufacturing and making the whole thing work and be sold to the market.   Genesi's main IP is their Aura firmware solution: http://www.genesi-usa.com/products/firmware   Aura, the Genesi Firmware offering, implements a run-time, re-entrant hardware abstraction layer supporting the industry standard IEEE 1275 (OpenFirmware) and UEFI firmware specifications, with significant added functionality.   These additional features provide cost reduction of systems and faster time-to-market of hardware. Genesi provides board bring-up services and firmware for other Power Architecture and ARM hardware suppliers, up to and including a Linux desktop, based on our firmware.   Genesi is an active Open Source supporter, having donated a lot of hardware over the years to Debian, OpenSuSe, Gentoo, Crux and many other Linux distributions.   Genesi says that they are very active in optimizing software specifically for ARM Cortex by porting libraries to the NEON unit in these devices resulting in large speedups.   Genesi has a developer forum: http://www.powerdeveloper.org Category: Science & Technology License: Standard YouTube License
View full article
DSC_0067 Added by iWavesystems on November 21, 2011 at 7:49am    
View full article
LinuxCon 2011 - Vancouver Added by Derald Woods on January 16, 2012 at 9:18pm   LinuxCon 2011 Gala
View full article
DSC_0054 Added by iWavesystems on April 3, 2012 at 8:40am    
View full article
DSC_0060 Added by iWavesystems on April 3, 2012 at 8:41am    
View full article
http://www.youtube.com/watch?feature=player_embedded&v=jGgNrrNctY8   Uploaded by mgrunditz on Jul 15, 2010 Now with hardware accelerated rendering. 45-55 FPS. Category: Science & Technology License: Standard YouTube License  
View full article
DSC_0034 Added by iWavesystems on November 21, 2011 at 7:47am    
View full article
2a Added by Ruslan on June 15, 2012 at 12:29pm    
View full article
APF28 up Added by Martoni on January 13, 2012 at 3:10am    
View full article
Technical Session Added by iWavesystems on June 26, 2012 at 3:45am    
View full article
http://www.youtube.com/watch?feature=player_embedded&v=R29iKVpyBOY   Uploaded by mgrunditz on Oct 27, 2010 Showing Efika MX Smarttop with Android. Viewing flash video from http://svtplay.se in window and fullscreen. Category: Science & Technology License: Standard YouTube License  
View full article
iWave @ Pedestal - 1112 , FTF-Americas Added by iWavesystems on June 18, 2012 at 4:15am   Be there to witness exciting Automotive solutions' demos...
View full article
DSC_0061 Added by iWavesystems on April 3, 2012 at 8:42am    
View full article
DSC_0074 Added by iWavesystems on April 3, 2012 at 8:58am    
View full article
DSC_0069 Added by iWavesystems on April 3, 2012 at 8:42am    
View full article