i.MX解决方案知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Solutions Knowledge Base

标签
  • General 294

讨论

排序依据:
http://www.youtube.com/watch?v=qSUE8K53mrI&feature=player_embedded   Uploaded by Charbax on Jun 23, 2011 Discussion with Linaro employees about the status of ARM Powered laptops. Category: Science & Technology License: Standard YouTube License  
查看全文
DIMM-MX535/DIMM-MX537 Added by Ramona Maurer on March 28, 2012 at 10:49am   Embedded Core modules based on i.MX535/i.MX537 (Cortex-A8), BSP for WEC 7.0, Linux, QNX available
查看全文
Technical Session Added by iWavesystems on June 26, 2012 at 3:53am    
查看全文
2a Added by Ruslan on June 15, 2012 at 12:29pm    
查看全文
Oraculo Added by Fábio Alves Oliveira Silva on July 1, 2011 at 8:59am    
查看全文
Added by Martin Welford on June 15, 2010 at 5:11am   http://www.youtube.com/watch?feature=player_embedded&v=svKqcE3KTcY   Uploaded by DeviceSolutionsLtd on Jun 14, 2010 Create small, smart, connected devices faster with the Topaz i.MX25 CPU module. http://devicesolutions.net/Products/TopaziMX25DevelopmentKit.aspx Category: Science & Technology License: Standard YouTube License  
查看全文
i.MX53 SOM at Arm TechCon,2011 Added by iWavesystems on November 17, 2011 at 7:21am    
查看全文
http://www.youtube.com/watch?feature=player_embedded&v=aED0x7_NptY   Uploaded by emtrion on Aug 24, 2011 processor modul showing parallel two videos using silverlight and vector graphic using Open VG Category: Science & Technology License: Standard YouTube License  
查看全文
Added by Johan Dams on June 24, 2010 at 7:07am   http://www.youtube.com/watch?feature=player_embedded&v=pOSluW6vHL8   Uploaded by Charbax on Jun 22, 2010 http://genesiamericas.com is presenting this awesome looking ARM Cortex A8 based Smartbook design, presented by Genesi who designed the hardware in collaboration with Pegatron of this latest generation of this Freescale Powered Smartbook design. For fun, we are running Microsoft Office through a high resolution version of Citrix viewer on the latest version of Ubuntu 10.4 for ARM processors. This could provide a one click online based software as a service solution. Want to run any X86 application on your ARM Laptop? Just click through the Citrix virtualization stuff and you can have it all running and smoothly. In theory, the apps could be processed by a grid and delivered much faster than on a single x86 processor based device.   Genesi are providing the hardware and software integration solution, in combination with Future Electronics, they can provide the whole solution to carriers, distributors, with the full bill of material, setting up the manufacturing and making the whole thing work and be sold to the market.   Genesi's main IP is their Aura firmware solution: http://www.genesi-usa.com/products/firmware   Aura, the Genesi Firmware offering, implements a run-time, re-entrant hardware abstraction layer supporting the industry standard IEEE 1275 (OpenFirmware) and UEFI firmware specifications, with significant added functionality.   These additional features provide cost reduction of systems and faster time-to-market of hardware. Genesi provides board bring-up services and firmware for other Power Architecture and ARM hardware suppliers, up to and including a Linux desktop, based on our firmware.   Genesi is an active Open Source supporter, having donated a lot of hardware over the years to Debian, OpenSuSe, Gentoo, Crux and many other Linux distributions.   Genesi says that they are very active in optimizing software specifically for ARM Cortex by porting libraries to the NEON unit in these devices resulting in large speedups.   Genesi has a developer forum: http://www.powerdeveloper.org Category: Science & Technology License: Standard YouTube License
查看全文
QBIT Running Linux - Matchbox Added by Renato Torres Tovar on January 7, 2012 at 8:58pm QBIT embedded system... I.MX23, 128LQFP    
查看全文
http://www.youtube.com/watch?v=AxqNOEPFtCk&feature=player_embedded   Uploaded by LinaroOrg on Nov 3, 2011 Orlando, Nov. 2, 2011   I took the opportunity of the Q4.11 edition of Linaro Connect to meet with 3 members of the Freescale Landing team at Linaro: Paul Liu (middleware and graphics acceleration), Haitao Zhang (kernel) and Eric Miao (tech lead, a long time contributor to the ARM Linux community).   In Linaro, a landing team is a engineering team that works on making a hardware platform supported in the upstream open-source projects such as the Linux kernel and distributions like Ubuntu and Android.   Eric, Paul and Haitao explained how they work with the Freescale engineers (they actually are employed by Canonical), and gave details about the technical challenges they face. It was also an opportunity to speak about the Freescale i.MX53 QuickStart board they work on, a low cost yet very powerful board for the community.   This board, together with the kernel and distribution releases made by Linaro, allows community contributors to work always with the latest versions. This is essential to allow the community to contribute.   They also explained how they work together. In particular, they organized a code sprint in Shanghai 1 month before, and had a very productive week together. Category: Science & Technology License: Creative Commons Attribution license (reuse allowed)  
查看全文
IMG_0627 Added by Vikas on April 20, 2012 at 3:24pm    
查看全文
QBIT Running Linux - xterm Added by Renato Torres Tovar on January 7, 2012 at 8:47pm  
查看全文
img-0004-fsl-ptx Added by Robert Schwebel on November 10, 2010 at 6:46pm   Bjoern Buerger from the Pengutronix team demonstrates a Qt 4.7 demo on the MX28.
查看全文
http://www.youtube.com/watch?v=oR3VeeiKAOw&feature=player_embedded   Uploaded by BoundaryDevices on Feb 15, 2011 Dual Displays running in Portrait Mode on an IMX515 processor. Our NitrogenE board is connected to an HDMI monitor and a 7" 800x480 TTL display. OS is Debian. Category: Science & Technology License: Standard YouTube License  
查看全文
http://www.youtube.com/watch?feature=player_embedded&v=jGgNrrNctY8   Uploaded by mgrunditz on Jul 15, 2010 Now with hardware accelerated rendering. 45-55 FPS. Category: Science & Technology License: Standard YouTube License  
查看全文
CPU: ARM Cortex-A9,FreeScale i.MX6Q1Ghz/1.2Ghz 1024M Byte  DDR3 SDRAM,4G BYTE eMMC Flash 5 usart , USB Host,USB OTG 124 bits TFT port ,dual LVDS output  and HDMI IIC*2,McSPI*3,CAN*2,SD card *3,6*6 keyboard 120 pin conn *2 FR4 PC size:84*55(mm)
查看全文
Hi,      I want to expand another 1000M/s ethernet using EIM or PCIE of i.mx6Q,is that ok? How I can do that?
查看全文
Trisendo 2D/3D Video Board Added by Leon Woestenberg on February 19, 2012 at 9:56am   The Trisendo Video Board mounts directly onto the i.MX53QSB.   Using FPGA video processing the reference design demonstrates 2D+Z to 3D rendering for 3D displays that do not require 3D glasses.  
查看全文
DSC_0055 Added by iWavesystems on April 3, 2012 at 8:40am    
查看全文